Other Parts Discussed in Thread: DAC7512, TLV320AIC3254, MIKROELEKTRONIKA
Hi guys! With some help from some of the fine folks on this forum a week or so ago I now have my TM4C123G working with this MAX549 8 bit DAC. I'm thrilled and can't thank you guys enough. I'm now trying to get it to work with a 12 bit DAC - the MAX5353. One problem: According to the datasheet it requires a reference input voltage of 1.5 Volts. This surprised me as the MAX549 doesn't have a REF IN pin.
After a good bit of Googling, the best I can tell is that I'm supposed to provide this 1.5 volt input and could possibly use something like this LM4041CILPR part paired with the 3.3v output of the TM4C123G and proper resistor to create this 1.5 volt reference input as depicted in Figure 15 of the datasheet here. Am I at least on the right track? ...It's odd to me the 8 bit DAC did not require this reference voltage but the 12 bit DAC does..