This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1231GH6PMI timer and interrupt



I tried to light up and off the LED PA0,1,2,3 and PF0,1,2,3 for every second, but it can't get into the interrupt.

It's my code, please check.


#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_uart.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/interrupt.h"
#include "driverlib/timer.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "grlib/grlib.h"
#include "driverlib/gpio.h"
#include "driverlib/gpio.c"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/sysctl.c"
#include "driverlib/systick.h"
#include "driverlib/uart.h"
#include "driverlib/uart.c"
#include "driverlib/adc.h"

int sys_status;
void IRQ_Timer0AIntHandler(void);

void
IRQ_Timer0AIntHandler(void)
{

MAP_IntMasterDisable();
MAP_TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);

switch (sys_status)
{


case 0:
MAP_GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_4, GPIO_PIN_4);
sys_status = 1;
break;
case 1:
MAP_GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_4, 0);
MAP_GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_5, GPIO_PIN_5);
sys_status = 2;
break;
case 2:
MAP_GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_5, 0);
MAP_GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_6, GPIO_PIN_6);
sys_status = 3;
break;
case 3:
MAP_GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_6, 0);
MAP_GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_7, GPIO_PIN_7);
sys_status = 4;
break;
case 4:
MAP_GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_7, 0);
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_0, GPIO_PIN_0);
sys_status = 5;
break;
case 5:
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_0, 0);
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, GPIO_PIN_1);
sys_status = 6;
break;
case 6:
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, 0);
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, GPIO_PIN_2);
sys_status = 7;
break;
case 7:
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0);
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3, GPIO_PIN_3);
sys_status = 8;
break;
case 8:
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3, 0);
sys_status = 0;
break;
default :
sys_status = 0;
break;
}
MAP_IntMasterEnable();


}

int
main(void)

MAP_SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);

MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART3);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART4);

MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);

MAP_GPIOPinConfigure(GPIO_PA0_U0RX);
MAP_GPIOPinConfigure(GPIO_PA1_U0TX);
MAP_GPIOPinConfigure(GPIO_PC4_U4RX);
MAP_GPIOPinConfigure(GPIO_PC5_U4TX);
MAP_GPIOPinConfigure(GPIO_PC6_U3RX);
MAP_GPIOPinConfigure(GPIO_PC7_U3TX);

HWREG(GPIO_PORTF_BASE + 0x520) = 0x4C4F434B;
HWREG(GPIO_PORTF_BASE + 0x524) = 0x00FF;
HWREG(GPIO_PORTF_BASE + 0x420) = 0x0000;
HWREG(GPIO_PORTF_BASE + 0x51C) = 0x001F;

MAP_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
MAP_GPIOPinTypeUART(GPIO_PORTC_BASE, GPIO_PIN_4 | GPIO_PIN_5);
MAP_GPIOPinTypeUART(GPIO_PORTC_BASE, GPIO_PIN_6 | GPIO_PIN_7);

MAP_GPIOPinTypeGPIOOutput(GPIO_PORTA_BASE, GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_6 | GPIO_PIN_7);
MAP_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3 | GPIO_PIN_4);

MAP_UARTConfigSetExpClk(UART0_BASE, MAP_SysCtlClockGet(), 9600,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));//115200


MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);

MAP_TimerDisable(TIMER0_BASE, TIMER_A);
MAP_TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC | TIMER_CFG_A_PERIODIC);
MAP_TimerLoadSet(TIMER0_BASE, TIMER_A, MAP_SysCtlClockGet());
MAP_TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
MAP_IntEnable(INT_TIMER0A);
MAP_TimerEnable(TIMER0_BASE, TIMER_A);

sys_status = 0;

while(1)
{
}

}