Other Parts Discussed in Thread: TMS570LC4357
We are in the process of troubleshooting an issue and would like to select VCLK to output on the ECLK1 pin of the TMS570LC4357. Table 6-18 in the datasheet lists the Clock Test Mode Options for Signals on ECLK1. SEL_ECP_PIN is defined as a 5 bit field, CLKTEST[4-0]. However the Clock Test Register in table 2-50 of the reference manual only provides a 4 bit field for SEL_ECP_PIN. Is this an error in the reference manual?
Is there sample code available to set up the ECLK1 pin?