Part Number: TMS570LS1227
Other Parts Discussed in Thread: HALCOGEN
Tool/software: TI C/C++ Compiler
Hi,
I read the Application report SPNA192 "UART Bootloader for Hercules TMS570LS12X MCU" and the associated code ( http://www.ti.com/lit/zip/spna192 ). However I am having an issue getting the board to respond to the SCI pins.
After compiling the code I simplified the void main( void ) function to have the following:
void main(void)
{
uint32_t fnRetValue;
uint32_t i=0;
/* Initialize SCI Routines to receive Command and transmit data */
sciInit();
UART_putString(UART, "\r\n Test ! ");
while(1){ }
}
Unfortunately I am unable to get the test serial message. In my (custom) board, I am using the SCI pins 38/39, and the serial communication works fine on normal applications (with all the registers set using Halcogen). When I debug the bootloader with my JTAG, I can definitely see that the code is being executed, except that the serial message is not being broadcast.
This is my void sciInit(void) function.
void sciInit(void)
{
/** @b intalise @b SCI1 */
unsigned f;
double vclk = SYS_CLK_FREQ * 1000000 / 2;
/** - bring SCI out of reset */
sciREG1->GCR0 = 0U;
sciREG1->GCR0 = 1U;
/** - Disable all interrupts */
sciREG1->CLRINT = 0xFFFFFFFF;
sciREG1->CLRINTLVL = 0xFFFFFFFF;
/** - global control 1 */
sciREG1->GCR1 = (1 << 25) /* enable transmit */
| (1 << 24) /* enable receive */
| (1 << 5) /* internal clock (device has no clock pin) */
| (0 << 4) /* number of stop bits */
| (0 << 3) /* even parity, otherwise odd */
| (0 << 2) /* enable parity */
| (1 << 1) /* asynchronous timing mode */
| (0 << 0);
/** - set baudrate */
// sciREG1->BAUD = 42; /* 115.20K baudrate for 160MHz Vclk */
// sciREG1->BAUD = 259; /* 19.2K baudrate for 160MHz Vclk */
// sciREG1->BAUD = 155; /* 19.2K baudrate for 96MHz Vclk */
f = sciREG1->GCR1 & 2 ? 16 : 1;
sciREG1->BAUD = ((unsigned)((vclk /(f*UART_BAUDRATE) + 0.5)) - 1) & 0x00FFFFFF;
sciREG1->BAUD = 259;
/** - tranmision length */
sciREG1->LENGTH = 7; /* length is 7+1 */
/** - set SCI pins functional mode */
sciREG1->FUN = (1 << 2) /* tx pin */
| (1 << 1) /* rx pin */
| (0); /* clk pin */
/** - set SCI pins default output value */
sciREG1->DOUT = (0 << 2) /* tx pin */
| (0 << 1) /* rx pin */
| (0); /* clk pin */
/** - set SCI pins output direction */
sciREG1->DIR = (0 << 2) /* tx pin */
| (0 << 1) /* rx pin */
| (0); /* clk pin */
/** - set SCI pins open drain enable */
sciREG1->ODR = (0 << 2) /* tx pin */
| (0 << 1) /* rx pin */
| (0); /* clk pin */
/** - set SCI pins pullup/pulldown enable */
sciREG1->PD = (0 << 2) /* tx pin */
| (0 << 1) /* rx pin */
| (0); /* clk pin */
/** - set SCI pins pullup/pulldown select */
sciREG1->PSL = (1 << 2) /* tx pin */
| (1 << 1) /* rx pin */
| (0); /* clk pin */
/** - set interrupt level */
sciREG1->SETINTLVL = (0 << 26) /* Framing error */
| (0 << 25) /* Overrun error */
| (0 << 24) /* Pariry error */
| (0 << 9) /* Receive */
| (0 << 8) /* Transmit */
| (0 << 1) /* Wakeup */
| (0); /* Break detect */
/** - set interrupt enable */
sciREG1->SETINT = (0 << 26) /* Framing error */
| (0 << 25) /* Overrun error */
| (0 << 24) /* Pariry error */
| (0 << 9) /* Receive */
| (0 << 1) /* Wakeup */
| (0); /* Break detect */
/** - inialise global transfer variables */
g_sciTransfer[0].mode = 0 << 8;
g_sciTransfer[0].length = 0;
/** - Finaly start SCI1 */
sciREG1->GCR1 |= 0x80;
}
It seems that the pins 38/39 are not being correctly assigned to the SCI RX/TX functionality. Can you guys help me out setting these up?