Hi,
We want to execute the SRAM PBIST on TMS570LC4357, then if there is a failure, we would like to get at what address that was and conversely guarantee that the first X bytes of the RAM have no failures. PBIST.RAMT register seems made for this since it identifies the RGS and RDS where the error occurred. The possible RGS and RDS are defined in "Table 2-5. PBIST Memory Grouping" of the TRM (SPNU563, May 2014). However,
1) We do not know to which portion of the SRAM "L2RAMW RGS #7" and "L2RAMW RGS #32" corresponds.
2) We do not know to which portion of the SRAM the various RDS corresponds.
Another mean we saw to achieve this is to use PBIST.FSRA0/1 registers which give the address of the first failure. However, we were wondering if the RAM PBIST was running sequentially. In other words, if that register gives the address Y, does this confirm that all addresses from RAM beginning to Y-1 have no failure?
Please help,
Etienne