This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TM4C1294NCPDT: Fault ISR - Precise Data Bus Error - Tiva C Series

Part Number: TM4C1294NCPDT

Tool/software: Code Composer Studio

Hello,

I am working in TM4C1294 launch pad, The program is running to FaultISR,

Following are the status found in debug mode

NVIC_FAULT_STAT_BFARV         1              Bus Fault Address Register Valid              

NVIC_FAULT_STAT_PRECISE      1              Precise Data Bus Error   

NVIC_FAULT_ADDR        0x432B546A        Bus Fault Address [Memory Mapped]   

I have referred for the memory mapping in the TM4C1294ncpdt data sheet.

The address in the register comes under Peripheral bit-band alias, what might be the issue that force the controller to fault ISR?