Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: EK-TM4C123GXL
Hi,
I am trying to program the TM4C device using lmflash CLI. The error message 0x1 keeps showing up.
I've searched E2E, and found many discussion about this issue. I've done:
1. Erase all command is ok.
2. Lower is frequency:
3. I've re-installed LM Flash Programmer but it is still failed.
Hardware: EK-TM4C123GXL
Firmware: USB_DEV_BULK adds dummy array to increase size (0x5CBC).
Software: LM Flash Programmer (Build 1613) on Windows 7 64-bit
Edward