Hello!
I will be handling multi-pin input. Apparently – packs of 8-20 bits pushed together at each clock. I attach the possible formats of input:
http://imgur.com/a/6yeYx
I'll bee needing 8 pins to drive a LED matrix. Which pixel-data input formats will I be able to support? 8-bit? 12, 16 or 20 bit? I think I can hit pin number limit with 20-pins.
Best regards,
Sebastian