Part Number: TM4C129XNCZAD
Hi e2e,
does there have any configuration in Tivaware graphic library for display rotation, 90,180,270?
i checked the user manual, there is no information about it.
thanks in advance.
LEON
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C129XNCZAD
Hi e2e,
does there have any configuration in Tivaware graphic library for display rotation, 90,180,270?
i checked the user manual, there is no information about it.
thanks in advance.
LEON
Hi Amit,
Static rotation is enough, do you have the related information?
thanks.
LEON
Hi Amit,
Yes, I found it, we can enable the define while compiling Graphic library.
// Although the display raster scans in a fixed direction with respect to a given origin, the raster display driver can be configured to rotate the
// displayed image to allow displays to be viewed in any portrait or landscape format. The orientation is selected at build time by defining one of
// NORMAL which orients the displayed image with the same origin as the raster scan, DISPLAY_ROTATE_90 which rotates the
// image such that the image origin is in the top right of the display with respect to the raster origin, DISPLAY_ROTATE_180 which places the image
// origin in the bottom right of the raster scan or DISPLAY_ROTATE_270 which places the origin at the bottom left of the raster. In the
// DISPLAY_ROTATE_90 and DISPLAY_ROTATE_270 cases, the width and height reported to the graphics library in the g_sGrRaster16BppDriver structure
// are reversed with respect to \b RASTER_WIDTH and \b RASTER_HEIGHT.
#ifdef DISPLAY_ROTATE_90
//
// This version of the function handles the cases where we are writing
// lines of pixels vertically downwards relative to the raster scan.
//
static void
GrRaster16BppDriverPixelDrawMultiple(void *pvDisplayData, int32_t lX,
int32_t lY, int32_t lX0, int32_t lCount,
int32_t lBPP, const uint8_t *pui8Data,
const uint8_t *pui8Palette)
{
uint16_t *pui16Ptr;
uint32_t ui32Byte;
tRaster16BppDriverInst *pInst;
int32_t lXMapped, lYMapped;
thanks.
LEON