This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Debug and Hibernation



Hello everyone,

I am working on a project where i have to transmit the sensor data through esp8266(wifi module) and go in hibernation for specified time. When the code runs for  1st time I am getting the values and controller goes in the hibernation. But when it comes out of hibernation it does not transmit and displays link is not valid. It also re-initiates the program instead of continuing with the flow.  I don't want to re-initiate and my data should go through esp after coming out from hibernation.

here is the part of my code

int main(void)
{
SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);

SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
HibernateEnableExpClk(SysCtlClockGet());

HibernateGPIORetentionEnable();
HibernateRTCEnable();
HibernateRTCSet(0);
HibernateRTCEnable();
HibernateRTCMatchSet(0,10);
HibernateWakeSet(HIBERNATE_WAKE_PIN | HIBERNATE_WAKE_RTC );

and after sending data through esp8266 i am  going in hibernation through HibernateRequest();

please review and help.

thank you in advance.