Part Number: TM4C123GH6PM
I wanted to use timers in TM4C123GH6PM (in TIVA C series TM4C123G Launchpad evaluation kit). So I decided to use GPTM TimerA0 in periodic timer mode. I defined the address of the
registers of GPTM and followed the steps given in the section 11.4.1 One-Shot/Periodic Timer Mode of the datasheet in page 722. I want a LED to blink after every 3 seconds (connected to
PORT F-pin 1). But the LED is always ON. Are the address of the registers to which I am referring wrong? Or something else is the issue with the code?
//TIMER Registers #define RCGCTIMER (*((volatile unsigned long *)0x400FE604)) #define GPTMCTL (*((volatile unsigned long *)0x4003000C)) //timer zero #define GPTMCFG (*((volatile unsigned long *)0x40030000)) #define GPTMTAMR (*((volatile unsigned long *)0x40030004)) #define GPTMTAILR (*((volatile unsigned long *)0x40030028)) #define GPTMRIS (*((volatile unsigned long *)0x4003001C)) #define GPTMICR (*((volatile unsigned long *)0x40030024)) //PORT F Registers #define GPIO_PORTF_LOCK_R (*((volatile unsigned long *)0x40025520)) #define GPIO_PORTF_DATA_R (*((volatile unsigned long*)0x400253FC)) #define GPIO_PORTF_DIR_R (*((volatile unsigned long *)0x40025400)) #define GPIO_PORTF_AFSEL_R (*((volatile unsigned long *)0x40025420)) #define GPIO_PORTF_DEN_R (*((volatile unsigned long *)0x4002551C)) #define SYSCTL2_RCGC2_R (*((volatile unsigned long *)0x400FE108)) #define SYSCTL_RCGC2_GPIOF 0x00000020 // port F Clock Gating Control void initializeTimer() { RCGCTIMER |= 0x00000001 ; //To use a GPTM, the appropriate TIMERn bit must be set in the RCGCTIMER. Here it is TIMER0 //Periodic timer mode GPTMCTL &=(~0x00000001); //TAEN is set 0. Timer A is disabled. GPTMCFG = 0x00000000; //Write the GPTM Configuration Register (GPTMCFG) with a value of 0x0000.0000 GPTMTAMR = 0x00000002; //TAMR is set 0x2. Periodic Timer mode is used (first bit1 is set 1 and then bit0 is set 0 in two statements) GPTMTAMR &= 0xFFFFFFEF; //TACDIR is set 0. The timer counts down. GPTMTAILR = 0x02DC6C00; //TAILR is set to 48,000,000 GPTMCTL |=0x00000001; //TAEN is set 1. Timer A is enabled. } void initializePORTF() { volatile unsigned long delay; SYSCTL2_RCGC2_R |= 0x00000020; // 1) F clock delay = SYSCTL2_RCGC2_R; // delay GPIO_PORTF_LOCK_R = 0x4C4F434B; // 2) unlock GPIO Port F GPIO_PORTF_DIR_R |= 0x02; // PF2 output GPIO_PORTF_AFSEL_R &= 0x00; // No alternate function// 1) F clock GPIO_PORTF_DEN_R |= 0x02; // Enable digital pins PF2 GPIO_PORTF_DATA_R |= 0x02; //PF1 Set to 1. LED is ON } int main() { initializeTimer(); initializePORTF(); while(1) { //did TATORIS in GPTMRIS become 1?? if((GPTMRIS | 0x00000001) == 1) { GPTMICR |= 0x00000001; //Set 1 to TATOCINT. Writing a 1 to this bit clears the TATORIS bit in the GPTMRIS register and the TATOMIS bit in the GPTMMIS register. GPIO_PORTF_DATA_R ^= 0x02; //Toggle PF1. Toggle LED } } }