Hello,
I am working with a Launchpad XL2 RM57Lx, I was able to program it via its XDS110 usb interface. When i returned after the weekend my computer was no longer able to detect it.
If I run C:\ti\ccsv7\ccs_base\common\uscif\xds110>xdsdfu -e
The output is:
Found 0 devices.
It also does not show up in the windows device manager.
I already tried to reinstall the drivers. Both the usb port and cable work correctly (tried with RM48HDK and works fine).
When i power the board the +5V LED6 next to the ethernet port is on.
Is my board broken? How can I reconnect to it?
I am using Code Composer Studio 7 on Windows 7.
Kind regards,
Karel