Hi
I have purchased DK-TM4C129X development kit.
I am not getting 3.3V at the test point.
If remove jumper j8, getting 3.3V at pin2 of j8.
Regards,
Kiran Shingote
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I have purchased DK-TM4C129X development kit.
I am not getting 3.3V at the test point.
If remove jumper j8, getting 3.3V at pin2 of j8.
Regards,
Kiran Shingote
Dear Amit,
Thanks for reply.
Yes, I run few programs from example folder.
I was providing power to DK-TM4C129X through USB.
One day morning, I connected USB cable and tried to upload program, could not upload.
Then I checked voltages and found 3.3V fault.
Regards,
Kiran Shingote
Dear Amit,
Thanks for reply,
Can you please suggest what shall I do ?
Regards,
Kiran Shingote
In contrast to, "un-soldering & removing devices" - might strategic, pcb trace slices - which interrupt (break) the flow of 3V3 - prove easier?
Firm/I have found that such "isolation" of components - commencing furthest down the power distribution trail/line - may more quickly identify the failed device... (i.e. break the 3V3 to an IC/component in which that breakage does not impact any other (or fewest other) board devices.)
In addition - should an "over-current" condition (really) be occurring - a fast responding & high resolution temperature probe should be able to note the source of such current.
Note that when removing power from a device (via the above, board slice method) it is vital to prevent voltage and/or signal introduction from arriving at any (other) pin of that IC...