This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HALCOGEN: HALCoGen 4.06.00 Crashes From Clock Tree Selection on General Tab

Part Number: HALCOGEN

Hi,

I have just installed HALCoGen 4.6.0 alongside previous 4.5.2 (which is still installed). I get a crash after creating a brand new project when selecting 'Clock Tree' from the General tab.

File > New > Project > TMS570LS1227PGE

Presented with General Tab, select 'Clock Tree'', get pop-up box stating:

HAL Code Generator has stopped working

A problem caused the program to stop working correctly. Windows will close the program and notify you if a solution is available.

I have tried to attach my project files that were created (.dil and .hcg) but this function doesn't appear to be working in my Chrome browser.

I am running Windows 7 service pack 1 on an Intel Core i7-3720QM CPU, 64-bit.

HALCoGen 4.5.2 works just fine.

Regards, Tony.