Part Number: TM4C1231H6PM
1. I want to use two 7-seg to count perasecond, but I can't turn on the 7-seg now, please help me check my code, maybe I lose something.
2. I have two 7-segment, how can I control them separately?
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_uart.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/interrupt.h"
#include "driverlib/timer.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/gpio.h"
#include "driverlib/gpio.c"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/sysctl.c"
#include "driverlib/systick.h"
#include "driverlib/uart.h"
#include "driverlib/uart.c"
#include "driverlib/adc.h"
int
main(void)
{
MAP_SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);
//
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
//
MAP_GPIOPinConfigure(GPIO_PA0_U0RX);
MAP_GPIOPinConfigure(GPIO_PA1_U0TX);
//
HWREG(GPIO_PORTF_BASE + 0x520) = 0x4C4F434B;
HWREG(GPIO_PORTF_BASE + 0x524) = 0x00FF;
HWREG(GPIO_PORTF_BASE + 0x420) = 0x0000;
HWREG(GPIO_PORTF_BASE + 0x51C) = 0x001F;
//
MAP_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
// 7-Seg_A : PB1 | 7-Seg_B : PD6 | 7-Seg_C : PF0
// 7-Seg_D : PF1 | 7-Seg_E : PF2 | 7-Seg_F : PB0
// 7-Seg_G : PD5
MAP_GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE, GPIO_PIN_0 | GPIO_PIN_1);
MAP_GPIOPinTypeGPIOOutput(GPIO_PORTD_BASE, GPIO_PIN_5 | GPIO_PIN_6);
MAP_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2);
//
MAP_UARTConfigSetExpClk(UART0_BASE, MAP_SysCtlClockGet(), 115200,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));
while(1)
{
MAP_GPIOPinWrite(GPIO_PORTB_BASE, GPIO_PIN_1, GPIO_PIN_1); //a
MAP_GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_6, GPIO_PIN_1); //b
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_0, GPIO_PIN_0); //c
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, GPIO_PIN_1); //d
MAP_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, GPIO_PIN_2); //e
MAP_GPIOPinWrite(GPIO_PORTB_BASE, GPIO_PIN_0, GPIO_PIN_0); //f
MAP_GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_5, GPIO_PIN_5); //g
}
}