Part Number: TMS570LC4357
Other Parts Discussed in Thread: TINA-TI
Hello,
in my project we are using TMS570LC4357 uC and we are using On-chip ADC channels to read the Analog input voltages, Input Voltage range is 0-24V, and there is a voltage divider circuit (ratio: 0.205) followed with a Op-amp voltage buffer circuit provided before ADC Input at uC. So the input to uC is 4.9V max. uC placed on a 10 layer PCB and the Voltage divider and buffer circuit provided in Another 8 Layer PCB. Both PCB's connected together by a Connector.
Issue Facing:
while we do ADC measurement, We are getting a Saw-Tooth pulse type noise pulse in ADC Channel input signal at between Voltage buffer o/p and uC input point. Refer the attachment.
1. we checked and found this noise pulse presents whenever the ADC sampling occurring, If we change the sampling time then the time difference between the noise pulse also changing.
2. if we increase the input voltage, the amplitude of the noise pulse also getting increase.
Due to this we are getting wrong ADC Value. Can anyone tell why this noise pulse occurring and how to avoid this....
Awaiting for your inputs.. thanks in advance.