Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
I am generating the drivers from HALCoGen for a simple DCAN_TX project. The following is my code:
/* USER CODE BEGIN (0) */
/* USER CODE END */
/* Include Files */
#include "HL_sys_common.h"
/* USER CODE BEGIN (1) */
#include "HL_can.h"
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
#define D_SIZE 9
uint8_t tx_data[D_SIZE] = {'H','E','R','C','U','L','E','S','\0'};
uint32_t checkPackets(uint8_t *src_packet, uint8_t *dst_packet, uint32_t psize);
/* USER CODE END */
int main(void)
{
/* USER CODE BEGIN (3) */
canInit();
canTransmit(canREG1, CANMESSAGE_BOX1, tx_data);
while(1);
/* USER CODE END */
return 0;
}
/* USER CODE BEGIN (4) */
uint32_t checkPackets(uint8_t *src_packet, uint8_t *dst_packet, uint32_t psize){
uint32_t err=0;
uint32_t cnt=psize;
while(cnt--){
if((*src_packet++) != (*dst_packet++))
err++;
}
return (err);
}
void canMessageNotification(canBASE_t *node, uint32_t messageBox)
{
return;
}
void canErrorNotification(canBASE_t *node, uint32_t notification)
{
return;
}
void esmGroup1Notification(unsigned channel)
{
return;
}
void esmGroup2Notification(unsigned channel)
{
return;
}
/* USER CODE END */
I am getting the following error:
#1965 cannot open source file "stdint.h"
which is included in the HL_hal_stdtypes.h file.