how to connect the TFT display
(ECTM4C1294xl) on which pins should I use
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Don't know this board/display, and the vendor's site seems down currently.
However, judged by the few pins, it is serial (SPI) only.
Not my favourite method, because:
Beside Bruno's concerns about the electrical interface, check out if this device fulfills your performance requirements.
As a starter, investigate the fastest method to write to several pixel values (sequence of SPI writes), and calculate how long a screen fill will take.
berat barlas said:how to connect the TFT display
Would not a better (and more important) question be, "Why START with so demanding a display & interface?"
"SIMPLE" starts build your knowledge, capability & experience. Overly complex ones (TFT) achieve, "Pain/Suffering/Delay/Frustration!"
A "nice" post appeared (right here) recently - suggesting FAR MORE SUITABLE Displays for a (clear) "first effort."
Indeed f.m. - indeed. Staff/I are (being entertained) watching ONE Large Character (painfully) draw upon an Arduino Controlled (word used lightly) TFT. Second cup (hot chocolate) and the "top half" of that character (may) be (almost) recognizable. (this w/the Ard. "cranked" - and running downhill...)
Kilimanjaro IS there - emits a (strong) siren call - yet not all should heed/succumb to such clear, "Over Challenge." (staff member here twisted her ankle climbing parking garage)
As always - KISS rules - even though - and especially though - that direction appears (near) "banned here!"
Swimming the English Channel "seems" easy! (right after I learn - How to swim...)
Mine too. In retrospect, I was quite naive then ...
And my "fate" there could not be compared to Elvis' military service - rather dealing with an AK-47 copy than a guitar.
BTW, since the OP seems still absent (or has abandoned this thread), we can go on indulging in digressions ...
f. m. said:Perhaps we have scared the OP away
Should not his "unschooled purchase" of a (most likely) soon to be orphaned, overly complex display - have (rightly) achieved that? NOT to be unkind - but really - KISS RULES!
Such beginners must be taught, "Always watch the magician's, "Off Hand."" (that's where the REAL action occurs...)