Part Number: TMS570LC4357
I made a simple CAN_TX code where I am transmitting "HERCULES" through CAN4 through message box 1, but I am unable to compile my code and having the following errors:
Description Resource Path Location Type
gmake: Target 'all' not remade because of errors. DCAN_TX C/C++ Problem
gmake: *** [source/HL_system.obj] Error 1 DCAN_TX C/C++ Problem
gmake: *** [source/HL_sys_vim.obj] Error 1 DCAN_TX C/C++ Problem
gmake: *** [source/HL_sys_startup.obj] Error 1 DCAN_TX C/C++ Problem
gmake: *** [source/HL_sys_pmm.obj] Error 1 DCAN_TX C/C++ Problem
gmake: *** [source/HL_sys_phantom.obj] Error 1 DCAN_TX C/C++ Problem
gmake: *** [source/HL_sys_pcr.obj] Error 1 DCAN_TX C/C++ Problem
gmake: *** [source/HL_sys_main.obj] Error 1 DCAN_TX C/C++ Problem
gmake: *** [source/HL_sys_dma.obj] Error 1 DCAN_TX C/C++ Problem
gmake: *** [source/HL_pinmux.obj] Error 1 DCAN_TX C/C++ Problem
gmake: *** [source/HL_notification.obj] Error 1 DCAN_TX C/C++ Problem
gmake: *** [source/HL_nmpu.obj] Error 1 DCAN_TX C/C++ Problem
gmake: *** [source/HL_esm.obj] Error 1 DCAN_TX C/C++ Problem
gmake: *** [source/HL_errata.obj] Error 1 DCAN_TX C/C++ Problem
gmake: *** [source/HL_epc.obj] Error 1 DCAN_TX C/C++ Problem
gmake: *** [source/HL_can.obj] Error 1 DCAN_TX C/C++ Problem
#66 expected a ";" .ccsproject /DCAN_TX line 49, external location: C:\ti\ccsv6\tools\compiler\arp32_1.0.8\include\_lock.h C/C++ Problem
#66 expected a ";" .ccsproject /DCAN_TX line 50, external location: C:\ti\ccsv6\tools\compiler\arp32_1.0.8\include\_lock.h C/C++ Problem
#262-D explicit type is missing ("int" assumed) .ccsproject /DCAN_TX line 49, external location: C:\ti\ccsv6\tools\compiler\arp32_1.0.8\include\_lock.h C/C++ Problem
#262-D explicit type is missing ("int" assumed) .ccsproject /DCAN_TX line 50, external location: C:\ti\ccsv6\tools\compiler\arp32_1.0.8\include\_lock.h C/C++ Problem
#112-D statement is unreachable HL_sys_main.c /DCAN_TX/source line 81 C/C++ Problem
and the following is my main code:
/* USER CODE BEGIN (0) */
/* USER CODE END */
/* Include Files */
#include "HL_sys_common.h"
/* USER CODE BEGIN (1) */
#include "HL_can.h"
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
#define D_SIZE 9
uint8_t tx_data[D_SIZE] = {'H','E','R','C','U','L','E','S','\0'};
uint32_t checkPackets(uint8_t *src_packet, uint8_t *dst_packet, uint32_t psize);
/* USER CODE END */
int main(void)
{
/* USER CODE BEGIN (3) */
canInit();
canTransmit(canREG4, canMESSAGE_BOX1, tx_data);
while(1);
/* USER CODE END */
return 0;
}
/* USER CODE BEGIN (4) */
uint32_t checkPackets(uint8_t *src_packet, uint8_t *dst_packet, uint32_t psize){
uint32_t err=0;
uint32_t cnt=psize;
while(cnt--){
if((*src_packet++) != (*dst_packet++))
err++;
}
return (err);
}
void canMessageNotification(canBASE_t *node, uint32_t messageBox)
{
return;
}
void canErrorNotification(canBASE_t *node, uint32_t notification)
{
return;
}
void esmGroup1Notification(unsigned channel)
{
return;
}
void esmGroup2Notification(unsigned channel)
{
return;
}
/* USER CODE END */