This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DK-TM4C123G: Set up CAN demo on DK-TM4C123G

Part Number: DK-TM4C123G

Hi,

I am trying to set up CAN demo on two DK-TM4C123G demo boards. I have added two 120ohm resistors to both sides. The data did send from TX side and I can measure it on CAN wire. I also measure the signal between CAN transceiver and MCU (RX side), and I can see the data. I assume the demo code is correct so I did not change anything to the example project. Is there anything I should do?

Regards,

Edward