Part Number: TMS570LS0714
Other Parts Discussed in Thread: HALCOGEN
Hello All,
My customer uses MibSPI both for connections with another TMS570LS0714 and connections with 3p MCU at 20MHz.
TMS570LS0714- TMS570LS0714 connection: Oscillogram shows a pause between 16-bit packages. Everything is OK.
When the customer tries to connect TMS570LS0714 with 3p MCU then there is on pause between 16-bit packages, the customer does not see any solution how to setup the pause. And in case of connection faster than 3MHz the connection crashes completely. If connection speed is lower than 3MHz then in RX register of MibSPI all words are marked by overflow bit RXOVR, but data is correct.