This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294NCPDT: TM4C1294NCPDT

Part Number: TM4C1294NCPDT


HI sir,

 we download the Led and UART code in to TM4C1294NCPDT launchpad that is working good. I added SSI code to led and uart code now I try to download the code in to launchpad  using LM flash programer tool but it is not happens.

I am using LM flash programer tool to download the code.

please find the below link for video.

drive.google.com/open

I used below code.

please find below code. 


#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/gpio.h"
#include "drivers/pinout.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
#include "driverlib/ssi.h"
#include "inc/hw_ssi.h"
#include "driverlib/debug.h"
#include "inc/hw_sysctl.h"
#include "inc/hw_types.h"

//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>Hello World (hello)</h1>
//!
//! A very simple ``hello world'' example. It simply displays ``Hello World!''
//! on the UART and is a starting point for more complicated applications.
//!
//! Open a terminal with 115,200 8-N-1 to see the output for this demo.
//
//*****************************************************************************

//*****************************************************************************
//
// System clock rate in Hz.
//
//*****************************************************************************
uint32_t g_ui32SysClock;

//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif

//*****************************************************************************
//
// Configure the UART and its pins. This must be called before UARTprintf().
//
//*****************************************************************************
void
ConfigureUART(void)
{
//
// Enable the GPIO Peripheral used by the UART.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

//
// Enable UART0
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);

//
// Configure GPIO Pins for UART mode.
//
ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);

//
// Initialize the UART for console I/O.
//
UARTStdioConfig(0, 115200, g_ui32SysClock);
}


void
SSIConfigSetExpClk(uint32_t ui32Base, uint32_t ui32SSIClk,
uint32_t ui32Protocol, uint32_t ui32Mode,
uint32_t ui32BitRate, uint32_t ui32DataWidth)
{
uint32_t ui32MaxBitRate;
uint32_t ui32RegVal;
uint32_t ui32PreDiv;
uint32_t ui32SCR;
uint32_t ui32SPH_SPO;

//
// Check the arguments.
//
ASSERT(_SSIBaseValid(SSI0_BASE));
ASSERT((ui32Protocol == SSI_FRF_MOTO_MODE_0) ||
(ui32Protocol == SSI_FRF_MOTO_MODE_1) ||
(ui32Protocol == SSI_FRF_MOTO_MODE_2) ||
(ui32Protocol == SSI_FRF_MOTO_MODE_3) ||
(ui32Protocol == SSI_FRF_TI) ||
(ui32Protocol == SSI_FRF_NMW));
ASSERT((ui32Mode == SSI_MODE_MASTER) ||
(ui32Mode == SSI_MODE_SLAVE));
ASSERT(((ui32Mode == SSI_MODE_MASTER) &&
(ui32BitRate <= (ui32SSIClk / 2))) ||
((ui32Mode != SSI_MODE_MASTER) &&
(ui32BitRate <= (ui32SSIClk / 12))));
ASSERT((ui32SSIClk / ui32BitRate) <= (254 * 256));
ASSERT((ui32DataWidth >= 4) && (ui32DataWidth <= 16));

//
// Set the mode.
//
ui32RegVal = (ui32Mode == SSI_MODE_MASTER) ? 0 : SSI_CR1_MS;
HWREG(SSI0_BASE + SSI_O_CR1) = ui32RegVal;

//
// Set the clock predivider.
//
ui32MaxBitRate = ui32SSIClk / ui32BitRate;
ui32PreDiv = 0;
do
{
ui32PreDiv += 2;
ui32SCR = (ui32MaxBitRate / ui32PreDiv) - 1;
}
while(ui32SCR > 255);
HWREG(SSI0_BASE + SSI_O_CPSR) = ui32PreDiv;

//
// Set protocol and clock rate.
//
ui32SPH_SPO = (ui32Protocol & 3) << 6;
ui32Protocol &= SSI_CR0_FRF_M;
ui32RegVal = (ui32SCR << 8) | ui32SPH_SPO | ui32Protocol |
(ui32DataWidth - 1);
HWREG(SSI0_BASE + SSI_O_CR0) = ui32RegVal;
}


void
SSIEnable(uint32_t ui32Base)
{
//
// Check the arguments.
//
ASSERT(_SSIBaseValid(ui32Base));

//
// Read-modify-write the enable bit.
//
HWREG(ui32Base + SSI_O_CR1) |= SSI_CR1_SSE;

}


void
SSIDataPut(uint32_t ui32Base, uint32_t ui32Data)
{
//
// Check the arguments.
//
ASSERT(_SSIBaseValid(ui32Base));
ASSERT((ui32Data & (0xfffffffe << (HWREG(ui32Base + SSI_O_CR0) &
SSI_CR0_DSS_M))) == 0);

//
// Wait until there is space.
//
while(!(HWREG(ui32Base + SSI_O_SR) & SSI_SR_TNF))
{
}

//
// Write the data to the SSI.
//
HWREG(ui32Base + SSI_O_DR) = ui32Data;
}

//*****************************************************************************
//
// Print "Hello World!" to the UART on the Intelligent UART Module.
//
//*****************************************************************************
int
main(void)
{

//
// Run from the PLL at 120 MHz.
//
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN | SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);

//
// Configure the device pins.
//
PinoutSet(false, false);


//
// Enable the GPIO pins for the LED D1 (PN1).
//
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_1);

//
// Initialize the UART.
//
ConfigureUART();

//
// Initialize the SSI0.
//
SSIEnable(SSI0_BASE);
SSIConfigSetExpClk(SSI0_BASE, 50000000, SSI_FRF_MOTO_MODE_0,SSI_MODE_MASTER, 1000000, 8);


SSIDataPut(SSI0_BASE, 'B');

//
// Hello!
//
while(1)
{
//UARTprintf(" uart code!\n");

SSIDataPut(SSI0_BASE, 0x55);
//
// We are finished. Hang around flashing D1.
//

//
// Turn on D1.
//
LEDWrite(CLP_D1, 1);


//
// Delay for a bit.
//
SysCtlDelay(g_ui32SysClock / 10 / 3);

//
// Turn off D1.
//
LEDWrite(CLP_D1, 0);

//
// Delay for a bit.
//
SysCtlDelay(g_ui32SysClock / 10 / 3);


}

}