Part Number: EK-TM4C1294XL
Other Parts Discussed in Thread: BOOSTXL-CC2650MA, CC2650,
I plan to develop a CC2650 bluetooth module communication with a TM4C129x board. To speed up the process, I'd rather start by using the boosterpack BOOSTXL-CC2650MA, which comes with such module.
TI's online tool "BoosterPack Checker" says it is not compatible, for PIN#35 is PC-6/WT1CCP0 on the lauchpad, while the boosterpack requires a RST wiring into the MCU.
Does the "obvious" workaround apply? Can I simply cut away pin #35 from the launchpad, and wire the pin#35 of the booster into the RST line of the TM4C board? Or is there something else REALLY specific to the MSP43x family which is required for that booster, that I'm not seeing here?
Regards
Bruno