This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM48L952: Load program Error - Does not match the target endianness

Genius 13655 points

Part Number: RM48L952

Dear Champs,

MCU : RM48L952 Rev. D(RM48L952DZWTT)

CCS : V7.0.0.00043

Debug probe : XDS2xx USB

Device endianness setting in CCS : little

  

Load program Error(Does not match the target endianness, not loaded) occurs.

However, the little endianness setting is no problem with "RM48L952 Rev. C"

 
Customer checked c1, System Control Register.

"RM48L952 Rev. C" : 0x09E70879 (bit[31] identified little-endianness)

"RM48L952 Rev. D" : 0x8BE70879 (bit[31] identified big-endianness)

 

RM48x TRM says,

"1.3.1 For the TI RM48x family, the endianness has been configured to little-endian."

 
Q1. Does "RM48L952 Rev. D" have big-endianness configuration?

Q2. Is the endianness configuration built-in(fixed)? Or, could I change it?

Thanks.

Rgds
Shine