Part Number: TM4C1294KCPDT
Hi,
I am using TM4C1294KCPDT MCU as Telnet Client using IP address 10.100.5.142 and trying to connect with server IP 192.168.0.253. But i am not able to ping with Server. My subnet mask is 255.0.0.0 and gateway address is 0. When i change my server IP to same class as of Client, it starts pinging. What is the issue with different class of IP addresses of Client and Server?
All suggestions are highly appreciated. Thanks
Best Regards,
Amit Deswal