Part Number: TMS570LS0714
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
Hello team,
I am currently working with the TMS570LS0714PZ and am experiencing some odd behavior with pin 93.
I want to use this pin as an input GPIO with the N2HET1[17] function. To do this I need to mux the pin to its alternate function, N2HET1[17], and mux the N2HET1[17] function to pin 93. The latter mux is based on table 4-39 in the datasheet.
However, the first time I read the HETDIN register, the pin is always read as low, regardless of whether or not the pin is low or high. When I read the pin the second time, I get the correct reading. I noticed that any read or write of an N2HET register after muxing the N2HET1[17] function to pin 93 corrects the issue.
I do not experience this behavior on any other N2HET1 pin. I did not see any notes on this issue in the errata. Do you know of any odd behavior associated with muxing functions to alternate pins? Thanks!