Part Number: EK-TM4C123GXL
Tool/software: TI C/C++ Compiler
Hi Community,
I have a Problem Programming the MC.
I modified the example Project project0 to print via UART for debbuging - this works quite fine.
Then I added a function (in a new source file) added it to the makefile and everything needed to do and just let this function print out a sentence over UART - this works as well.
Now comes the interesting part. I initialize an array (the dots just fill a long sentence):
uint8_t message_str[281] = "...."
Then i let a pointer point to the array
uint8_t * message = &message_str[0];
I hand over the ponter to my function, but i do not use it!! If i compile and flash my code via makefile I get no error message but if i flash it to the MC (with lm4flash) the MC does literally nothing.
But when i reduce the size of the array for example to 120 (uint8_t message_str[120] = "....") and compile the code and flash it it works!!!!
I am desperate and happy for any help!!
Thanks in Advance!
Nate