Part Number: EK-TM4C123GXL
I am new to programming the LaunchPad and have been trying to figure out how to output data/strings to my computer console. I am mainly using minicom in Linux, but I have also tried using PuTTY in Windows 10. Neither produce any output. I've read through the utils/uartstdio.c and utils/uartstdio.h source code and simply cannot figure out what I am missing. Any help would be much appreciated.
Just FYI, I did make sure that minicom and PuTTY were configured for 115200 bps.
The following is my code:
#include <stdbool.h>
#include <stdint.h>
#include "stdlib.h"
#include <stdio.h>
#include "inc/hw_types.h"
#include "inc/hw_gpio.h"
#include "inc/hw_memmap.h"
#include "inc/hw_sysctl.h"
#include "inc/hw_uart.h"
#include "driverlib/gpio.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/pin_map.h"
#include "driverlib/can.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.c"
#define LED_RED GPIO_PIN_1
#define LED_BLUE GPIO_PIN_2
#define LED_GREEN GPIO_PIN_3
void initialize();
void cycle_lights();
int main()
{
ROM_SysCtlClockSet(SYSCTL_SYSDIV_4|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, LED_RED|LED_BLUE|LED_GREEN);
ROM_GPIOPinTypeGPIOInput(GPIO_PORTA_BASE, GPIO_PIN_5);
// Settings for UARTprintf
ROM_UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
ROM_GPIOPinTypeUART(GPIO_PORTB_BASE, GPIO_PIN_0|GPIO_PIN_1);
UARTStdioConfig(0, 115200, MAP_SysCtlClockGet());
UARTprintf("DATA INIT");
initialize();
for (;;)
{
int32_t btn = ROM_GPIOPinRead(GPIO_PORTA_BASE, GPIO_PIN_5);
UARTprintf("btn %ld\n",btn);
if(btn != 0)
{
cycle_lights();
}
}
}
void initialize()
{
ROM_GPIOPinWrite(GPIO_PORTF_BASE, LED_RED|LED_GREEN|LED_BLUE, LED_GREEN);
}
void cycle_lights()
{
ROM_SysCtlDelay(50000000);
ROM_GPIOPinWrite(GPIO_PORTF_BASE, LED_RED, LED_RED);
ROM_SysCtlDelay(50000000);
ROM_GPIOPinWrite(GPIO_PORTF_BASE, LED_RED|LED_GREEN|LED_BLUE, LED_RED);
ROM_SysCtlDelay(100000000);
ROM_GPIOPinWrite(GPIO_PORTF_BASE, LED_RED|LED_GREEN|LED_BLUE, LED_GREEN);
}
EDIT: Tried to reorder some things and make it a bit more readable....
EDIT:
- changed UARTStdioConfig(0, 115200, MAP_SysCtlClockGet());" back to "UARTStdioConfig(0, 115200, 16000000);" per Amit's advice.
- Attempted to include "utils/uartstdio.c" via the Makefile, rather than in main.c (see Makefile below).
Here is my Makefile, if it helps diagnosis:
# /tiva-template/Makefile with added source uartstdio.c
# TARGET: name of the output file
TARGET = main
# MCU: part number to build for
MCU = TM4C123GH6PM
# SOURCES: list of input source sources
SOURCES = main.c startup_gcc.c uartstdio.c
# INCLUDES: list of includes, by default, use Includes directory
INCLUDES = -IInclude
# OUTDIR: directory to use for output
OUTDIR = build
# TIVAWARE_PATH: path to tivaware folder
TIVAWARE_PATH = $(HOME)/Embedded/tivaware
# LD_SCRIPT: linker script
LD_SCRIPT = $(MCU).ld
# define flags
CFLAGS = -g -mthumb -mcpu=cortex-m4 -mfpu=fpv4-sp-d16 -mfloat-abi=softfp
CFLAGS +=-Os -ffunction-sections -fdata-sections -MD -std=c99 -Wall
CFLAGS += -pedantic -DPART_$(MCU) -c -I$(TIVAWARE_PATH)
CFLAGS += -DTARGET_IS_BLIZZARD_RA1
LDFLAGS = -T $(LD_SCRIPT) --entry ResetISR --gc-sections
#######################################
# end of user configuration
#######################################
#
#######################################
# binaries
#######################################
CC = arm-none-eabi-gcc
LD = arm-none-eabi-ld
OBJCOPY = arm-none-eabi-objcopy
RM = rm -f
MKDIR = mkdir -p
#######################################
# list of object files, placed in the build directory regardless of source path
OBJECTS = $(addprefix $(OUTDIR)/,$(notdir $(SOURCES:.c=.o)))
# default: build bin
all: $(OUTDIR)/$(TARGET).bin
$(OUTDIR)/%.o: src/%.c | $(OUTDIR)
$(CC) -o $@ $^ $(CFLAGS)
$(OUTDIR)/a.out: $(OBJECTS)
$(LD) -o $@ $^ $(LDFLAGS)
$(OUTDIR)/main.bin: $(OUTDIR)/a.out
$(OBJCOPY) -O binary $< $@
# create the output directory
$(OUTDIR):
$(MKDIR) $(OUTDIR)
clean:
-$(RM) $(OUTDIR)/*
.PHONY: all clean