Part Number: TMS570LS3134
Other Parts Discussed in Thread: TMS320F28335, , TMS570LC4357
Hello,
one of my customers is asking about the performance of the TMS570LS3134 compared to the TMS320F28335.
On their current project they are using the TMS320F28335 for a motor control application. Now, their requirements changed to ASIL-D and ISO26262 and therefore they are considering the TMS570LS3134 for their new design.
The current implementation with the C2000 is almost on its limit. The new implementation is basically the same. The TMS320 is stated as 150MIPS and the TMS570 with almost 300DMIPS (180MHz times 1.66DMIPS/MHz), are these numbers comparable in this application?
Can you please help me out with that?
Thank you and kind regards,
Felix