Hi,
My device handle an SD.
Is it possible to update the firmware from SD via SSI?
What do the functions in Section 35.4 of the Peripheral Controller Library do?
What do the functions in Chapter 3 of the TivaWare Boot Loader User Guide do?
Is it possible to use boot_demo1 with boot_serial on an SD via SSI? Without having to use the LM Flash Programmer
Thanks in advance
Andrés