Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: EK-TM4C1294XL, , UNIFLASH, LMFLASHPROGRAMMER, TIDM-TM4C129POEAUDIO
Tool/software: Code Composer Studio
Dear sir,
We purchased the EK-TM4C1294XL Board and we want to dump code in it using XDS100V2 using JTAG configuration.
Could you please guide how to do this using XDS100V2 with JTAG.I dont want to use U6 present on the Board i want to directly Program the U1 without using U20.
I referred to the below link but the issue did not solve and we removed the R8,R10,R11,R15,R16 and installed XI also but we are getting error.

error :
FATAL >> CS_DAP_0: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.83.1
Requesting to please suggest how i can dump the code in EVAL BOARD using the Jtag not using U6 and U20.
we need this because we designed 1 board in which we are using the TM4C1294NCPDT in that JTAG is detecting but unable to dump the Code in it.so we are trying the sample program first in evaluation board only.
Regards,
Vipin