Other Parts Discussed in Thread: HALCOGEN,
I have doubts about possibility of instruction tracing on the TMS570LS31 Hercules™ Development Kit. The doubts come from my little experience with configuring TPIU register (see error -1170 forum thread). I found that it is impossible to write and even read the Current Port Size Register (offset 0x004) and by default it is set after reset to 0x00000001 (bus width). I know this from the 8.6.2 chapter of CoreSight Components Technical Reference Manual and from the behavior observed on the digital analyzer connected to the MIPI60 port. When I enable the TPIU Pattern Generator for generating then I observe that:
- for walking 1's pattern the ETMDATA[0] has 3.3V other pins are grounded
- for walking 0's pattern all pins are grounded
- for AA/55 pattern and FF/00 pattern only the ETMDATA[0] alternates each cycle like the clock
Could anybody confirm this?
Regards, Radek