This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137: About ADC3 MibADC Information Redundancy Techniques

Part Number: TMS570LS3137

Is this Information Redundancy saying to add CRC etc. when holding the converted value in RAM?

  • Hello,

    Yes this could be one interpretation. You could also consider the redundant ADC cores using the same analog signal as an input. Note that some of the ADC pins automatically have redundant paths to ADC1 and again to ADC2 on the same pin. Since both paths operate on the same analog signal, it is considered information redundancy.