Part Number: LAUNCHXL2-RM57L
Hi,
I am building a project with Arduino (slave) and Launchpad Rm57L (master) to get data from Arduino and send it to Http server.
I cant get data from I2C.I have not Analyzer because i build a Arduino for i2c sniffer and there is no data on i2c line.
I am using example code for RM57 and 2 4.7k pull-up resistor for i2c line.i2c line connected to J1 header 9 and 10 ports.
And this github.com/.../i2c-sniffer-100kBaud-Arduino-Mega for Arduino.Rm57 code get stuck in
while(i2cIsBusBusy(i2cREG1) == true);
infinite loop.
int main(void)
{
/* USER CODE BEGIN (3) */
int repeat = 0; int delay =0;
///////////////////////////////////////////////////////////////
// Master Transfer Functionality //
///////////////////////////////////////////////////////////////
/* I2C Init as per GUI
* Mode = Master - Transmitter
* baud rate = 100KHz
* Count = 10
* Bit Count = 8bit
*/
i2cInit();
/* Configure address of Slave to talk to */
i2cSetSlaveAdd(i2cREG1, Slave_Address);
/* Set direction to Transmitter */
/* Note: Optional - It is done in Init */
i2cSetDirection(i2cREG1, I2C_TRANSMITTER);
for(repeat = 0; repeat < 2; repeat++)
{
/* Configure Data count */
/* Note: Optional - It is done in Init, unless user want to change */
i2cSetCount(i2cREG1, DATA_COUNT);
/* Set mode as Master */
i2cSetMode(i2cREG1, I2C_MASTER);
/* Set Stop after programmed Count */
i2cSetStop(i2cREG1);
/* Transmit Start Condition */
i2cSetStart(i2cREG1);
/* Tranmit DATA_COUNT number of data in Polling mode */
i2cSend(i2cREG1, DATA_COUNT, TX_Data_Master);
/* Wait until Bus Busy is cleared */
while(i2cIsBusBusy(i2cREG1) == true);
/* Wait until Stop is detected */
while(i2cIsStopDetected(i2cREG1) == 0);
/* Clear the Stop condition */
i2cClearSCD(i2cREG1);
/* Simple Dealya before starting Next Block */
/* Depends on how quick the Slave gets ready */
for(delay=0;delay<1000000;delay++);
}
///////////////////////////////////////////////////////////////
// Master Receive Functionality //
///////////////////////////////////////////////////////////////
/* Configure address of Slave to talk to */
i2cSetSlaveAdd(i2cREG1, Slave_Address);
/* Set direction to receiver */
i2cSetDirection(i2cREG1, I2C_RECEIVER);
for(repeat = 0; repeat < 2; repeat++)
{
/* Configure Data count */
/* Note: Optional - It is done in Init, unless user want to change */
i2cSetCount(i2cREG1, DATA_COUNT);
/* Set mode as Master */
i2cSetMode(i2cREG1, I2C_MASTER);
/* Set Stop after programmed Count */
i2cSetStop(i2cREG1);
/* Transmit Start Condition */
i2cSetStart(i2cREG1);
/* Tranmit DATA_COUNT number of data in Polling mode */
i2cReceive(i2cREG1, DATA_COUNT, RX_Data_Master);
/* Wait until Bus Busy is cleared */
while(i2cIsBusBusy(i2cREG1) == true);
/* Wait until Stop is detected */
while(i2cIsStopDetected(i2cREG1) == 0);
/* Clear the Stop condition */
i2cClearSCD(i2cREG1);
/* Simple Dealya before starting Next Block */
/* Depends on how quick the Slave gets ready */
for(delay=0;delay<1000000;delay++);
}
asm(" nop");
asm(" nop");
asm(" nop");
while(1);
/* USER CODE END */
return 0;
}