Tool/software: TI C/C++ Compiler
HI,
I am working with with the TM4c123G MCU, and the kentec booster pack board. I have gone through a lot to try and make it work and it is still not working. I am using lab 10 from TI to just get it up and running right now. I have removed R9 and R10, and added the SPI for this touch screen. I am not sure if i added them correctly? i saved them to the folder TI>TivaWare2.1.3.156>Examples>boards>kentec. I also copied them into the file that had the 8.bit code. I am not sure if i did that correct? i also set up all the file search paths correctly. the error I'm getting now is this. Any suggestions??