Part Number: TM4C123GH6PM
Hi everyone. I'm a very begining student with the ARM-based microcontrollers, so one, for a developement of a project I chose the TM4C123GH6PM. I have a Stellaris LM4F120 LaunchPad EK, and I pretend to use it like a programmer for the Tiva. But I don't know if it's possible to use one to program the other one. And, if I should have to write the code using the Stellarisware or the Tivaware. Other point that I have doubt is about the ADC pins, if they support inputs with 3.3V or 5V. Any suggestion will be very important. Thank you.