Part Number: TM4C123GH6PM
hello , i have a tiva C microcontroller and i was working on a project of interfacing an adxl 345 accelerometer sensor with it using I2C i have managed to get it working using a clock of 80 MHZ and using the PLL to set the clock of the I2C module to 100 and it is working perfectly fine if i use step by step debugging , however , if i run the program i get zeroes on the MDR register and the variables that i read the data from MDR register into
step by step debugging gives clear and CORRECT results my problem is when letting the program to run it gives all zeroes
if i try to step debug after that it will keep the zeroes and i have to disconnect the sensor's power and reconnect it for it to work again , i dont know why this is happening any help ? is the clock too much at 80 MHZ or what ?
things i have tried:
i have tried adding some software delay to act as a step by step debugging between each read and write operation and still it didnt work and gave me zeroes again.
here is my code in case it is needed
#include "tm4c123gh6pm.h"
#include "stdint.h"
void EnableI2CModule0(void);
uint8_t ReadRegister(uint8_t RegisterAddress);
void PLL_Init(void);
void WriteRegister(uint8_t RegisterAddress,uint8_t Data);
volatile uint8_t X_Axis1,X_Axis2,Y_Axis1,Y_Axis2,Z_Axis1,Z_Axis2=0;
int main()
{
volatile long temp;
PLL_Init();
EnableI2CModule0();
temp=ReadRegister(0x00);
WriteRegister(0x2D,0x08);
temp=ReadRegister(0x2D);
WriteRegister(0x31,0x0B);
temp=ReadRegister(0x31);
while(1)
{
X_Axis1=ReadRegister(0x32);
X_Axis2=ReadRegister(0x33);
Y_Axis1=ReadRegister(0x34);
Y_Axis2=ReadRegister(0x35);
Z_Axis1=ReadRegister(0x36);
Z_Axis2=ReadRegister(0x37);
}
}
void PLL_Init(void){
// 0) Use RCC2
SYSCTL_RCC2_R |= 0x80000000; // USERCC2
// 1) bypass PLL while initializing
SYSCTL_RCC2_R |= 0x00000800; // BYPASS2, PLL bypass
// 2) select the crystal value and oscillator source
SYSCTL_RCC_R = (SYSCTL_RCC_R &~0x000007C0) // clear XTAL field, bits 10-6
+ 0x00000540; // 10101, configure for 16 MHz crystal
SYSCTL_RCC2_R &= ~0x00000070; // configure for main oscillator source
// 3) activate PLL by clearing PWRDN
SYSCTL_RCC2_R &= ~0x00002000;
// 4) set the desired system divider
SYSCTL_RCC2_R |= 0x40000000; // use 400 MHz PLL
SYSCTL_RCC2_R = (SYSCTL_RCC2_R&~ 0x1FC00000) // clear system clock divider
+ (4<<22); // configure for 80 MHz clock
// 5) wait for the PLL to lock by polling PLLLRIS
while((SYSCTL_RIS_R&0x00000040)==0){}; // wait for PLLRIS bit
// 6) enable use of PLL by clearing BYPASS
SYSCTL_RCC2_R &= ~0x00000800;
}
void EnableI2CModule0(void)
{
volatile int Delay=0;
SYSCTL_RCGCI2C_R|=0x00000001; //set i2c module 0 clock active
Delay=SYSCTL_RCGCI2C_R; //delay allow clock to stabilize
SYSCTL_RCGCGPIO_R |=0x00000002; //i2c module 0 is portB so activate clock for port B
Delay = SYSCTL_RCGCGPIO_R; //delay allow clock to stabilize
GPIO_PORTB_AFSEL_R|= 0x0000000C; //enable alternate functions for PB2 and PB3
GPIO_PORTB_ODR_R |= 0x00000008; //set PB3 (I2C SDA) for open drain
GPIO_PORTB_DEN_R |= 0xFF; //Enable digital on Port B
GPIO_PORTB_PCTL_R |=0x03;
I2C0_PP_R |= 0x01;
I2C0_MTPR_R |= 0x00000027; //set SCL clock
I2C0_MCR_R |= 0x00000010; //intialize mcr rigester with that value given in datasheet
}
uint8_t ReadRegister(uint8_t RegisterAddress)
{
volatile uint8_t result=0;
I2C0_MSA_R = 0x000000A6; //write operation
I2C0_MDR_R = RegisterAddress; //place data to send mdr register
I2C0_MCS_R = 0x00000007; //stop start run
while((I2C0_MCS_R &= 0x00000040)==1); //poll busy bit
I2C0_MSA_R = 0x000000A7; // read operation
I2C0_MCS_R = 0x00000007; // stop start run
while((I2C0_MCS_R &= 0x00000040)==1); //poll busy bit
result = I2C0_MDR_R;
return result;
}
void WriteRegister(uint8_t RegisterAddress,uint8_t Data)
{
I2C0_MSA_R = 0x000000A6; //write operation
I2C0_MDR_R = RegisterAddress; //place register address to set in mdr register
I2C0_MCS_R = 0x00000003; //burst send ( multiple bytes send )
while((I2C0_MCS_R &= 0x00000040)==1); //poll busy bit
I2C0_MDR_R = Data; //place data to be sent in mdr register
I2C0_MCS_R = 0x00000005; // transmit followed by stop state
while((I2C0_MCS_R &= 0x00000040)==1); //poll busy bit
}