Part Number: EK-TM4C1294XL
Tool/software: Code Composer Studio
Hi,
I'm trying to use the Hibernate RTC module to keep track of time, but when I set the interrupt time, instead of interrupting every 60 seconds, it seems that is interrupting many times faster (really, MANY times faster). Also, after setting up RTC I cannot exit the program by pressing enter, it "resets" the program everytime I do that. I've tried to copy similar examples from the internet, but it always gives me the same behaviour.
What might cause this? I'm configuring interrupts the wrong way?
/*
* adc.c
*
* Created on: 24 de jan de 2017
* Author: Helder Sales
*/
#include "adc.h"
#include "../wdog/wdog.h"
#include "../../includes.h"
#include "../../../command/read/read.h"
//To verify char
unsigned char ch;
//Number of input pins and type
uint8_t numarg, Inputs, pinPE, pinPK;
//Time
uint8_t minute, hour;
inline unsigned char ADC_InitADCPins(char *g_cInput)
{
//argv
static char *argv[8 + 1];
char *pcChar;
uint_fast8_t argc = 0;
bool bFindArg = true;
pcChar = g_cInput;
while(*pcChar)
{
if(*pcChar == ' ')
{
*pcChar = 0;
bFindArg = true;
}
else if(bFindArg)
{
argv[argc] = pcChar;
argc++;
bFindArg = false;
}
pcChar++;
}
char *num = argv[1];
unsigned int aux;
uint8_t condition = sscanf(num, "%u%c", &aux, &ch);
pinPE = strcmp(argv[0], "PE");
pinPK = strcmp(argv[0], "PK");
numarg = argc;
Inputs = aux;
if((pinPE != 0 && pinPK != 0) || condition != 1)
{
Inputs = 0;
return(Inputs);
}
//Enable pin J
ROM_SysCtlPeripheralDisable(SYSCTL_PERIPH_GPIOJ);
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_GPIOJ);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOJ);
while(!ROM_SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOJ));
//Configures pin PJ0 as input
ROM_GPIOPinTypeGPIOInput(GPIO_PORTJ_BASE, GPIO_PIN_0);
//General config (pull-up)
GPIOPadConfigSet(GPIO_PORTJ_BASE, GPIO_PIN_0, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU);
if(pinPE == 0)
{
//Enable pin E
ROM_SysCtlPeripheralDisable(SYSCTL_PERIPH_GPIOE);
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_GPIOE);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
while(!ROM_SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOE));
if(Inputs == 1)
//Enable pin PE0 as ADC
ROM_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_0);
if(Inputs == 2)
//Enable pin PE0/PE1 as ADC
ROM_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_0 | GPIO_PIN_1);
if(Inputs == 3)
//Enable pin PE0/PE1/PE2 as ADC
ROM_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2);
if(Inputs == 4)
//Enable pin PE0/PE1/PE2/PE3 as ADC
ROM_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3);
}
else if(pinPK == 0)
{
//Enable pin K
ROM_SysCtlPeripheralDisable(SYSCTL_PERIPH_GPIOK);
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_GPIOK);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOK);
while(!ROM_SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOK));
if(Inputs == 1)
//Enable pin PK0 as ADC
ROM_GPIOPinTypeADC(GPIO_PORTK_BASE, GPIO_PIN_0);
if(Inputs == 2)
//Enable pin PK0/PK1 as ADC
ROM_GPIOPinTypeADC(GPIO_PORTK_BASE, GPIO_PIN_0 | GPIO_PIN_1);
if(Inputs == 3)
//Enable pin PK0/PK1/PK2 as ADC
ROM_GPIOPinTypeADC(GPIO_PORTK_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2);
if(Inputs == 4)
//Enable pin PK0/PK1/PK2/PK3 as ADC
ROM_GPIOPinTypeADC(GPIO_PORTK_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3);
}
return(Inputs);
}
inline void ADC_InitADC(unsigned char Inputs, unsigned char oversamplevalue)
{
//Enable ADC0
ROM_SysCtlPeripheralDisable(SYSCTL_PERIPH_ADC0);
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_ADC0);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
while(!ROM_SysCtlPeripheralReady(SYSCTL_PERIPH_ADC0));
//Enable ADC1
ROM_SysCtlPeripheralDisable(SYSCTL_PERIPH_ADC1);
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_ADC1);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC1);
while(!ROM_SysCtlPeripheralReady(SYSCTL_PERIPH_ADC1));
//Configures ADC0 sequence 2, trigger by the processor, priority 0 (highest)
ROM_ADCSequenceConfigure(ADC0_BASE, 2, ADC_TRIGGER_PROCESSOR, 0);
//Configures ADC1 sequence 3, trigger by the processor, priority 1
ROM_ADCSequenceConfigure(ADC1_BASE, 3, ADC_TRIGGER_PROCESSOR, 1);
//Step 0 sequence 2, MCU's temp sampling, sequence (0 to the highest), configures interrupt after sampling, tells ADC1 this is the last conversion
ROM_ADCSequenceStepConfigure(ADC1_BASE, 3, 0, ADC_CTL_TS | ADC_CTL_IE | ADC_CTL_END);
if(pinPE == 0)
{
if(Inputs == 1)
{
//Step 0 sequence 2, sampling of channel 0, sequence (0 to the highest), configures interrupt after sampling, tells ADC that CH19 is the last conversion
//(to know more about channels, see datasheet pg. 1056)
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 0, ADC_CTL_CH3 | ADC_CTL_IE | ADC_CTL_END);
}
else if(Inputs == 2)
{
//Step 0 sequence 2, sampling of channel 0/1, sequence (0 to the highest), configures interrupt after sampling, tells ADC that CH19 is the last conversion
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 0, ADC_CTL_CH3);
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 1, ADC_CTL_CH2 | ADC_CTL_IE | ADC_CTL_END);
}
else if(Inputs == 3)
{
//Step 0 sequence 2, sampling of channel 0/1/2, sequence (0 to the highest), configures interrupt after sampling, tells ADC that CH19 is the last conversion
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 0, ADC_CTL_CH3);
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 1, ADC_CTL_CH2);
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 2, ADC_CTL_CH1 | ADC_CTL_IE | ADC_CTL_END);
}
else if(Inputs == 4)
{
//Step 0 sequence 2, sampling of channel 0/1/2/3, sequence (0 to the highest), configures interrupt after sampling, tells ADC that CH19 is the last conversion
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 0, ADC_CTL_CH3);
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 1, ADC_CTL_CH2);
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 2, ADC_CTL_CH1);
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 3, ADC_CTL_CH0 | ADC_CTL_IE | ADC_CTL_END);
}
}
else if(pinPK == 0)
{
if(Inputs == 1)
{
//Step 0 sequence 2, sampling of channel 16, sequence (0 to the highest), configures interrupt after sampling, tells ADC that CH19 is the last conversion
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 0, ADC_CTL_CH16 | ADC_CTL_IE | ADC_CTL_END);
}
else if(Inputs == 2)
{
//Step 0 sequence 2, sampling of channel 16/17, sequence (0 to the highest), configures interrupt after sampling, tells ADC that CH19 is the last conversion
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 0, ADC_CTL_CH16);
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 1, ADC_CTL_CH17 | ADC_CTL_IE | ADC_CTL_END);
}
else if(Inputs == 3)
{
//Step 0 sequence 2, sampling of channel 16/17/18, sequence (0 to the highest), configures interrupt after sampling, tells ADC that CH19 is the last conversion
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 0, ADC_CTL_CH16);
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 1, ADC_CTL_CH17);
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 2, ADC_CTL_CH18 | ADC_CTL_IE | ADC_CTL_END);
}
else if(Inputs == 4)
{
//Step 0 sequence 2, sampling of channel 16/17/18/19, sequence (0 to the highest), configures interrupt after sampling, tells ADC that CH19 is the last conversion
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 0, ADC_CTL_CH16);
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 1, ADC_CTL_CH17);
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 2, ADC_CTL_CH18);
ROM_ADCSequenceStepConfigure(ADC0_BASE, 2, 3, ADC_CTL_CH19 | ADC_CTL_IE | ADC_CTL_END);
}
}
//Configures the ADC to 2MSPS (PLL/15 = 32MHz, Sampling rate full)
ADCClockConfigSet(ADC0_BASE, ADC_CLOCK_SRC_PLL | ADC_CLOCK_RATE_FULL, 15);
//Configures the ADC to 125KSPS (PLL/30 = 16MHz, Sampling rate 1/8th)
ADCClockConfigSet(ADC1_BASE, ADC_CLOCK_SRC_PLL | ADC_CLOCK_RATE_EIGHTH, 30);
//Oversampling (mean of samples, effective speed = (MSPS)*(oversample value))
ROM_ADCHardwareOversampleConfigure(ADC0_BASE, oversamplevalue);
ROM_ADCHardwareOversampleConfigure(ADC1_BASE, 64);
//habilita ADC0 sequence 2
ROM_ADCSequenceEnable(ADC0_BASE, 2);
//habilita ADC1 sequence 3
ROM_ADCSequenceEnable(ADC1_BASE, 3);
}
inline void ADC_InitHibernateRTC(void)
{
//Enable Hibernation Module
ROM_SysCtlPeripheralDisable(SYSCTL_PERIPH_HIBERNATE);
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_HIBERNATE);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_HIBERNATE);
while(!ROM_SysCtlPeripheralReady(SYSCTL_PERIPH_HIBERNATE));
ROM_HibernateEnableExpClk(120000000);
ROM_HibernateClockConfig(HIBERNATE_OSC_HIGHDRIVE);
ROM_HibernateRTCSet(0);
ROM_HibernateRTCMatchSet(0, 60);
ROM_HibernateIntEnable(HIBERNATE_INT_RTC_MATCH_0);
HibernateIntRegister(HibernateRTCIntHandler);
}
inline void Init_Timer1(unsigned int freq)
{
//Enable Timer 1
ROM_SysCtlPeripheralDisable(SYSCTL_PERIPH_TIMER1);
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_TIMER1);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER1);
while(!ROM_SysCtlPeripheralReady(SYSCTL_PERIPH_TIMER1));
//Timer 1 clock = PIOSC
ROM_TimerClockSourceSet(TIMER1_BASE, TIMER_CLOCK_PIOSC);
ROM_TimerConfigure(TIMER1_BASE, TIMER_CFG_PERIODIC);
uint32_t uiPeriod = 16000000/freq;
ROM_TimerLoadSet(TIMER1_BASE, TIMER_A, uiPeriod -1);
ROM_IntPrioritySet(INT_TIMER1A, 1);
ROM_IntEnable(INT_TIMER1A);
ROM_TimerIntEnable(TIMER1_BASE, TIMER_TIMA_TIMEOUT);
ROM_TimerEnable(TIMER1_BASE, TIMER_A);
}
void Timer1IntHandler(void)
{
ROM_TimerIntClear(TIMER1_BASE, TIMER_TIMA_TIMEOUT);
//Array with the length of the FIFO used (ver datasheet pag. 1056)
uint32_t ADC0Values[4];
uint32_t ADC1Values[1];
//Convert ADC value to temp
uint8_t TempValueC;
//Convert ADC0Values to voltage
uint16_t Value1, Value2, Value3, Value4;
static uint16_t Value1max = 0;
static uint16_t Value2max = 0;
static uint16_t Value3max = 0;
static uint16_t Value4max = 0;
static uint16_t Value1min = 4095*0.8058608059;
static uint16_t Value2min = 4095*0.8058608059;
static uint16_t Value3min = 4095*0.8058608059;
static uint16_t Value4min = 4095*0.8058608059;
//Clears ADC interrupt status
ROM_ADCIntClear(ADC0_BASE, 2);
ROM_ADCIntClear(ADC1_BASE, 3);
//Enable the triggers for the conversion
ROM_ADCProcessorTrigger(ADC0_BASE, 2);
ROM_ADCProcessorTrigger(ADC1_BASE, 3);
//Waits the conversion to be completed
while(!ROM_ADCIntStatus(ADC0_BASE, 2, false) || !ROM_ADCIntStatus(ADC1_BASE, 3, false));
//Reads the values obtained by the ADC
ROM_ADCSequenceDataGet(ADC0_BASE, 2, ADC0Values);
ROM_ADCSequenceDataGet(ADC1_BASE, 3, ADC1Values);
//Converts ADC values to temperature
TempValueC = (uint8_t)(147.5 - ((75.0 * 3.3 * (float)ADC1Values[0])) / 4096.0);
if(Inputs == 4)
{
//Converts ADC values to voltage
Value1 = ADC0Values[0]*0.8058608059;
Value2 = ADC0Values[1]*0.8058608059;
Value3 = ADC0Values[2]*0.8058608059;
Value4 = ADC0Values[3]*0.8058608059;
if(Value1max < Value1)
Value1max = Value1;
if(Value2max < Value2)
Value2max = Value2;
if(Value3max < Value3)
Value3max = Value3;
if(Value4max < Value4)
Value4max = Value4;
if(Value1min > Value1)
Value1min = Value1;
if(Value2min > Value2)
Value2min = Value2;
if(Value3min > Value3)
Value3min = Value3;
if(Value4min > Value4)
Value4min = Value4;
if(pinPE == 0)
//Print ADC results
UARTprintf("PE0 reading = %04u mV || Max. PE0 = %04u mV || Min. PE0 = %04u mV\n"
"PE1 reading = %04u mV || Max. PE1 = %04u mV || Min. PE1 = %04u mV\n"
"PE2 reading = %04u mV || Max. PE2 = %04u mV || Min. PE2 = %04u mV\n"
"PE3 reading = %04u mV || Max. PE3 = %04u mV || Min. PE3 = %04u mV\n\n"
"Elapsed time: %02uhrs %02umin %02usec MCU Temp: %u*C\x1b[5A\r", Value1, Value1max, Value1min, Value2, Value2max, Value2min,
Value3, Value3max, Value3min, Value4, Value4max, Value4min, hour, minute, ROM_HibernateRTCGet(), TempValueC);
else
UARTprintf("PK0 reading = %04u mV || Max. PK0 = %04u mV || Min. PK0 = %04u mV\n"
"PK1 reading = %04u mV || Max. PK1 = %04u mV || Min. PK1 = %04u mV\n"
"PK2 reading = %04u mV || Max. PK2 = %04u mV || Min. PK2 = %04u mV\n"
"PK3 reading = %04u mV || Max. PK3 = %04u mV || Min. PK3 = %04u mV\n\n"
"Elapsed time: %02uhrs %02umin %02usec MCU Temp: %u*C\x1b[5A\r", Value1, Value1max, Value1min, Value2, Value2max, Value2min,
Value3, Value3max, Value3min, Value4, Value4max, Value4min, hour, minute, ROM_HibernateRTCGet(), TempValueC);
}
else if(Inputs == 3)
{
//Converts ADC values to voltage
Value1 = ADC0Values[0]*0.8058608059;
Value2 = ADC0Values[1]*0.8058608059;
Value3 = ADC0Values[2]*0.8058608059;
if(Value1max < Value1)
Value1max = Value1;
if(Value2max < Value2)
Value2max = Value2;
if(Value3max < Value3)
Value3max = Value3;
if(Value1min > Value1)
Value1min = Value1;
if(Value2min > Value2)
Value2min = Value2;
if(Value3min > Value3)
Value3min = Value3;
if(pinPE == 0)
//Print ADC results
UARTprintf("PE0 reading = %04u mV || Max. PE0 = %04u mV || Min. PE0 = %04u mV\n"
"PE1 reading = %04u mV || Max. PE1 = %04u mV || Min. PE1 = %04u mV\n"
"PE2 reading = %04u mV || Max. PE2 = %04u mV || Min. PE2 = %04u mV\n\n"
"Elapsed time: %02uhrs %02umin %02usec MCU Temp: %u*C\x1b[4A\r", Value1, Value1max, Value1min, Value2, Value2max, Value2min,
Value3, Value3max, Value3min, hour, minute, ROM_HibernateRTCGet(), TempValueC);
else
//Print ADC results
UARTprintf("PK0 reading = %04u mV || Max. PK0 = %04u mV || Min. PK0 = %04u mV\n"
"PK1 reading = %04u mV || Max. PK1 = %04u mV || Min. PK1 = %04u mV\n"
"PK2 reading = %04u mV || Max. PK2 = %04u mV || Min. PK2 = %04u mV\n\n"
"Elapsed time: %02uhrs %02umin %02usec MCU Temp: %u*C\x1b[4A\r", Value1, Value1max, Value1min, Value2, Value2max, Value2min,
Value3, Value3max, Value3min, hour, minute, ROM_HibernateRTCGet(), TempValueC);
}
else if(Inputs == 2)
{
//Converts ADC values to voltage
Value1 = ADC0Values[0]*0.8058608059;
Value2 = ADC0Values[1]*0.8058608059;
if(Value1max < Value1)
Value1max = Value1;
if(Value2max < Value2)
Value2max = Value2;
if(Value1min > Value1)
Value1min = Value1;
if(Value2min > Value2)
Value2min = Value2;
if(pinPE == 0)
//Print ADC results
UARTprintf("PE0 reading = %04u mV || Max. PE0 = %04u mV || Min. PE0 = %04u mV\n"
"PE1 reading = %04u mV || Max. PE1 = %04u mV || Min. PE1 = %04u mV\n\n"
"Elapsed time: %02uhrs %02umin %02usec MCU Temp: %u*C\x1b[3A\r", Value1, Value1max, Value1min, Value2, Value2max, Value2min,
hour, minute, ROM_HibernateRTCGet(), TempValueC);
else
//Print ADC results
UARTprintf("PK0 reading = %04u mV || Max. PK0 = %04u mV || Min. PK0 = %04u mV\n"
"PK1 reading = %04u mV || Max. PK1 = %04u mV || Min. PK1 = %04u mV\n\n"
"Elapsed time: %02uhrs %02umin %02usec MCU Temp: %u*C\x1b[3A\r", Value1, Value1max, Value1min, Value2, Value2max, Value2min,
hour, minute, ROM_HibernateRTCGet(), TempValueC);
}
else if(Inputs == 1)
{
//Converts ADC values to voltage
Value1 = ADC0Values[0]*0.8058608059;
if(Value1max < Value1)
Value1max = Value1;
if(Value1min > Value1)
Value1min = Value1;
if(pinPE == 0)
//Print ADC results
UARTprintf("PE0 reading = %04u mV || Max. PE0 = %04u mV || Min. PE0 = %04u mV\n\n"
"Elapsed time: %02uhrs %02umin %02usec MCU Temp: %u*C\x1b[2A\r", Value1, Value1max, Value1min, hour, minute, ROM_HibernateRTCGet(), TempValueC);
else
//Print ADC results
UARTprintf("PK0 reading = %04u mV || Max. PK0 = %04u mV || Min. PK0 = %04u mV\n\n"
"Elapsed time: %02uhrs %02umin %02usec MCU Temp: %u*C\x1b[2A\r", Value1, Value1max, Value1min, hour, minute, ROM_HibernateRTCGet(), TempValueC);
}
if(Value1min == 0 && ROM_SysCtlPeripheralReady(SYSCTL_PERIPH_WDOG0))
{
FeedWatchdog = false;
while(1);
}
}
void HibernateRTCIntHandler(void)
{
ROM_HibernateIntClear(HIBERNATE_INT_RTC_MATCH_0);
minute++;
if(minute == 60)
{
hour++;
minute = 0;
}
ROM_HibernateRTCSet(0);
HibernateRTCMatchSet(0, 60);
}
inline void ADC_Loop(unsigned int freq)
{
hour = 0;
minute = 0;
UARTFlushRx();
Init_Timer1(freq);
ADC_InitHibernateRTC();
ROM_HibernateRTCEnable();
while(UARTPeek('\r') == -1);
UARTFlushRx();
ROM_IntDisable(INT_TIMER1A);
ROM_HibernateIntDisable(HIBERNATE_INT_RTC_MATCH_0);
ROM_TimerIntClear(TIMER1_BASE, TIMER_TIMA_TIMEOUT);
ROM_HibernateIntClear(HIBERNATE_INT_RTC_MATCH_0);
ROM_TimerDisable(TIMER1_BASE, TIMER_A);
HibernateIntUnregister();
ROM_SysCtlPeripheralDisable(SYSCTL_PERIPH_HIBERNATE);
ROM_SysCtlPeripheralDisable(SYSCTL_PERIPH_GPIOE);
ROM_SysCtlPeripheralDisable(SYSCTL_PERIPH_GPIOJ);
ROM_SysCtlPeripheralDisable(SYSCTL_PERIPH_ADC0);
ROM_SysCtlPeripheralDisable(SYSCTL_PERIPH_TIMER1);
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_GPIOE);
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_GPIOJ);
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_ADC0);
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_TIMER1);
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_HIBERNATE);
if(Inputs == 4)
UARTprintf("\n\n\n\n\n\nProgram terminated.\n");
if(Inputs == 3)
UARTprintf("\n\n\n\n\nProgram terminated.\n");
if(Inputs == 2)
UARTprintf("\n\n\n\nProgram terminated.\n");
if(Inputs == 1)
UARTprintf("\n\n\nProgram terminated.\n");
}
inline int ADC_main(int argc, char *argv[])
{
//text to indicate which pins are active
char text[8][32] = {"PE0", "PE0/PE1", "PE0/PE1/PE2", "PE0/PE1/PE2/PE3", "PK0", "PK0/PK1", "PK0/PK1/PK2", "PK0/PK1/PK2/PK3"};
unsigned int freq, oversamplevalue;
char *num1 = argv[1];
char *num2 = argv[3];
uint8_t condition = sscanf(num1, "%u%c", &freq, &ch);
if(freq <= 0 || argc == 1 || argc == 3 || argc > 4 || condition != 1)
return(CMD_ERROR);
else if(strcmp(argv[2], "oversample") == 0)
{
uint8_t condition2 = sscanf(num2, "%u%c", &oversamplevalue, &ch);
if((oversamplevalue == 2 || oversamplevalue == 4 || oversamplevalue == 8 || oversamplevalue == 16 || oversamplevalue == 32 || oversamplevalue == 64) && condition2 == 1)
{
UARTprintf("\nAnalog Digital Converter\n"
"Type: Single Ended.\n"
"Oversampling: %u\n"
"Update rate: %u Hz\n\n"
"Choose the port and the number of inputs (PE/PK, 1-4)\n\n"
">>", oversamplevalue, freq);
Read_Command();
Inputs = ADC_InitADCPins(g_cInput_Read());
ADC_InitADC(Inputs, oversamplevalue);
if(Inputs < 1 || Inputs > 4 || numarg > 2)
return(CMD_ERROR);
}
else if(condition2 != 1)
return(CMD_ERROR);
else
{
UARTprintf("\nOnly 2, 4, 8, 16, 32 and 64 are accepted for HW oversampling\n");
return(CMD_ERROR);
}
}
else if(argc == 2)
{
UARTprintf("\nAnalog Digital Converter\n"
"Type: Single Ended.\n"
"Oversampling: Deactivated\n"
"Update rate: %u Hz\n\n"
"Choose the port and the number of inputs (PE/PK, 1-4)\n\n"
">>", freq);
Read_Command();
Inputs = ADC_InitADCPins(g_cInput_Read());
ADC_InitADC(Inputs, 0);
if(Inputs < 1 || Inputs > 4 || numarg > 2)
return(CMD_ERROR);
}
if(pinPE == 0)
UARTprintf("\nNumber of inputs: %u\n"
"Inputs: %s\n\n"
"Press \"Enter\" or User Switch 1 to initiate.\n"
"After the program is running, press \"Enter\" again to exit.\n", Inputs, &text[Inputs-1]);
else
UARTprintf("\nNumber of inputs: %u\n"
"Inputs: %s\n\n"
"Press \"Enter\" or User Switch 1 to initiate.\n"
"After the program is running, press \"Enter\" again to exit.\n", Inputs, &text[Inputs+3]);
while(1)
{
//GPIOPinRead = 0 or GPIO_PIN_0
if(!ROM_GPIOPinRead(GPIO_PORTJ_BASE, GPIO_PIN_0))
{
UARTprintf("\n");
break;
}
if(UARTPeek('\r') != -1)
break;
}
ADC_Loop(freq);
return(CMD_SUCESS);
}