Part Number: EK-TM4C123GXL
Hello,
I tried to run GrLib examples on EK-TM4C123GXL launchpad with Kentec LCD booster pack, but I can't get to work any of the demos using buttons. The display works fine, scribble demo also works as expected, so hardware is not at fault. After a bit of debugging I managed to narrow down the issue to a chicken-and-an-egg problem in WidgetMessageSendPostOrder() function in file widget.c. The library was installed from file SW-TM4C-2.1.3.156.
Whom and how should I report the bug?
Thank you,
p.