Part Number: TMS570LS0714
Hello all,
Table 7-24 in the TMS570LS0714 datasheet lists the leakage currents for the device in on-state:
- Is this only when the ADC is connected and sampling, and if so what is the off-state input bias current
OR
- Is this continuous leakage per input pin when the ADC peripheral is turned on?
How are these values measured? By design? What are the statistics of these i.e. is this 3 sigma? 1 sigma? Are these a function of temperature, process, voltage?
Also - when the ADC is doing a conversion is the stated input current what it takes to charge the mux capacitors + sampling capacitor + current called out in 7-24 or does 7-24 take the mux and sampling capacitors into account? We have some high impedance sources driving the ADC – let’s say 3.3k resistor. If there is a leakage current that is called out in table 7-24, we will see 40LSBs of error due to the leakage current and one way to fix this is to add voltage followers/buffers and that is not reasonable in our design.
Thank you in advance!