Part Number: TM4C1290NCPDT
Tool/software: Code Composer Studio
Hi, I was using 4 timers to generate 4 square signals at diferent frequencies (8 9 10 and 11 KHz) from PC4 PC5 PC6 PC7 pins, every thing was ok, so I tried to use more timers to generate more square signals from other pins PH0 PH1 PH2 PH3 (8.5 9.5 10.5 and 11.5 KHz), so I tried to use the subtimers, here is the code:
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"+
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/timer.h"
//*****************************************************************************
uint32_t g_ui32SysClock; // System clock rate in Hz.
uint32_t g_ui32FlagsN; // Flags that contain the current value of the interrupt indicator as displayed on the UART.
uint32_t g_ui32FlagsF; // Flags that contain the current value of the interrupt indicator as displayed on the UART.
uint32_t g_ui32FlagsP; // Flags that contain the current value of the interrupt indicator as displayed on the UART.
uint32_t g_ui32FlagsB; // Flags that contain the current value of the interrupt indicator as displayed on the UART.
uint32_t g_ui32FlagsC; // Flags that contain the current value of the interrupt indicator as displayed on the UART.
uint32_t g_ui32FlagsH; // Flags that contain the current value of the interrupt indicator as displayed on the UART.
uint32_t leBandera = 0;
//*****************************************************************************
void Timer0IntHandler(void) // The interrupt handler for the first timer interrupt.
{
ROM_TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT); // Clear the timer interrupt.
HWREGBITW(&g_ui32FlagsN, 0) ^= 1; // Toggle the flag for the first timer.
HWREGBITW(&g_ui32FlagsC, 4) ^= 1; // Toggle the flag for the first timer.
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, g_ui32FlagsN); // Use the flags to Toggle the LED for this timer
GPIOPinWrite(GPIO_PORTC_BASE, GPIO_PIN_4, g_ui32FlagsC); // Use the flags to Toggle the LED for this timer
}
//*****************************************************************************
void Timer1IntHandler(void) // The interrupt handler for the second timer interrupt.
{
ROM_TimerIntClear(TIMER1_BASE, TIMER_TIMA_TIMEOUT); // Clear the timer interrupt.
HWREGBITW(&g_ui32FlagsN, 1) ^= 1; // Toggle the flag for the second timer.
HWREGBITW(&g_ui32FlagsC, 5) ^= 1; // Toggle the flag for the first timer.
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, g_ui32FlagsN); // Use the flags to Toggle the LED for this timer
GPIOPinWrite(GPIO_PORTC_BASE, GPIO_PIN_5, g_ui32FlagsC); // Use the flags to Toggle the LED for this timer
}
//*****************************************************************************
void Timer2IntHandler(void) // The interrupt handler for the second timer interrupt.
{
ROM_TimerIntClear(TIMER2_BASE, TIMER_TIMA_TIMEOUT); // Clear the timer interrupt.
HWREGBITW(&g_ui32FlagsF, 4) ^= 1; // Toggle the flag for the second timer.
HWREGBITW(&g_ui32FlagsC, 6) ^= 1; // Toggle the flag for the first timer.
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_4, g_ui32FlagsF); // Use the flags to Toggle the LED for this timer
GPIOPinWrite(GPIO_PORTC_BASE, GPIO_PIN_6, g_ui32FlagsC); // Use the flags to Toggle the LED for this timer
}
//*****************************************************************************
void Timer3IntHandler(void) // The interrupt handler for the second timer interrupt.
{
ROM_TimerIntClear(TIMER3_BASE, TIMER_TIMA_TIMEOUT); // Clear the timer interrupt.
HWREGBITW(&g_ui32FlagsF, 0) ^= 1; // Toggle the flag for the second timer.
HWREGBITW(&g_ui32FlagsC, 7) ^= 1; // Toggle the flag for the first timer.
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_0, g_ui32FlagsF); // Use the flags to Toggle the LED for this timer
GPIOPinWrite(GPIO_PORTC_BASE, GPIO_PIN_7, g_ui32FlagsC); // Use the flags to Toggle the LED for this timer
}
//*****************************************************************************
//*****************************************************************************
void Timer0IntHandlerB(void) // The interrupt handler for the first timer interrupt.
{
ROM_TimerIntClear(TIMER0_BASE, TIMER_TIMB_TIMEOUT); // Clear the timer interrupt.
HWREGBITW(&g_ui32FlagsH, 0) ^= 1; // Toggle the flag for the first timer.
GPIOPinWrite(GPIO_PORTH_BASE, GPIO_PIN_0, g_ui32FlagsH); // Use the flags to Toggle the LED for this timer
}
//*****************************************************************************
void Timer1IntHandlerB(void) // The interrupt handler for the second timer interrupt.
{
ROM_TimerIntClear(TIMER1_BASE, TIMER_TIMB_TIMEOUT); // Clear the timer interrupt.
HWREGBITW(&g_ui32FlagsH, 1) ^= 1; // Toggle the flag for the first timer.
GPIOPinWrite(GPIO_PORTH_BASE, GPIO_PIN_1, g_ui32FlagsH); // Use the flags to Toggle the LED for this timer
}
//*****************************************************************************
void Timer2IntHandlerB(void) // The interrupt handler for the second timer interrupt.
{
ROM_TimerIntClear(TIMER2_BASE, TIMER_TIMB_TIMEOUT); // Clear the timer interrupt.
HWREGBITW(&g_ui32FlagsH, 2) ^= 1; // Toggle the flag for the first timer.
GPIOPinWrite(GPIO_PORTH_BASE, GPIO_PIN_2, g_ui32FlagsH); // Use the flags to Toggle the LED for this timer
}
//*****************************************************************************
void Timer3IntHandlerB(void) // The interrupt handler for the second timer interrupt.
{
ROM_TimerIntClear(TIMER3_BASE, TIMER_TIMB_TIMEOUT); // Clear the timer interrupt.
HWREGBITW(&g_ui32FlagsH, 3) ^= 1; // Toggle the flag for the first timer.
GPIOPinWrite(GPIO_PORTH_BASE, GPIO_PIN_3, g_ui32FlagsH); // Use the flags to Toggle the LED for this timer
}
//*****************************************************************************
//*****************************************************************************
// This example application demonstrates the use of the timers to generate
// periodic interrupts.
//*****************************************************************************
int main(void)
{
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | // Set the clocking to run directly from the crystal at 120MHz.
SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION); // Enable the GPIO port that is used for the on-board LEDs.
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF); // Enable the GPIO port that is used for the on-board LEDs.
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC); // Enable the GPIO port that is used for the on-board LEDs.
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOH); // Enable the GPIO port that is used for the on-board LEDs.
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0 | GPIO_PIN_1); // Enable the GPIO pins for the LEDs (PN0 & PN1).
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_0 | GPIO_PIN_4);// Enable the GPIO pin for the LED (PF4).
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTC_BASE, GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_6 | GPIO_PIN_7);
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTH_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0); // Enable the peripherals used by this example.
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER1);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER2);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER3);
// ROM_IntMasterEnable(); // Enable processor interrupts.
TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC); // Configure the two 32-bit periodic timers.
TimerConfigure(TIMER1_BASE, TIMER_CFG_PERIODIC);
TimerConfigure(TIMER2_BASE, TIMER_CFG_PERIODIC);
TimerConfigure(TIMER3_BASE, TIMER_CFG_PERIODIC);
ROM_TimerLoadSet(TIMER0_BASE, TIMER_A, 2*(g_ui32SysClock/8000));
ROM_TimerLoadSet(TIMER1_BASE, TIMER_A, 2*(g_ui32SysClock/9000));
ROM_TimerLoadSet(TIMER2_BASE, TIMER_A, 2*(g_ui32SysClock/10000));
ROM_TimerLoadSet(TIMER3_BASE, TIMER_A, 2*(g_ui32SysClock/11000));
ROM_TimerLoadSet(TIMER0_BASE, TIMER_B, 2*(g_ui32SysClock/8500));
ROM_TimerLoadSet(TIMER1_BASE, TIMER_B, 2*(g_ui32SysClock/9500));
ROM_TimerLoadSet(TIMER2_BASE, TIMER_B, 2*(g_ui32SysClock/10500));
ROM_TimerLoadSet(TIMER3_BASE, TIMER_B, 2*(g_ui32SysClock/11500));
ROM_IntEnable(INT_TIMER0A); // Setup the interrupts for the timer timeouts.
ROM_IntEnable(INT_TIMER1A);
ROM_IntEnable(INT_TIMER2A);
ROM_IntEnable(INT_TIMER3A);
ROM_IntEnable(INT_TIMER0B);
ROM_IntEnable(INT_TIMER1B);
ROM_IntEnable(INT_TIMER2B);
ROM_IntEnable(INT_TIMER3B);
ROM_TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
ROM_TimerIntEnable(TIMER1_BASE, TIMER_TIMA_TIMEOUT);
ROM_TimerIntEnable(TIMER2_BASE, TIMER_TIMA_TIMEOUT);
ROM_TimerIntEnable(TIMER3_BASE, TIMER_TIMA_TIMEOUT);
ROM_TimerIntEnable(TIMER0_BASE, TIMER_TIMB_TIMEOUT);
ROM_TimerIntEnable(TIMER1_BASE, TIMER_TIMB_TIMEOUT);
ROM_TimerIntEnable(TIMER2_BASE, TIMER_TIMB_TIMEOUT);
ROM_TimerIntEnable(TIMER3_BASE, TIMER_TIMB_TIMEOUT);
ROM_TimerEnable(TIMER0_BASE, TIMER_A); // Enable the timers.
ROM_TimerEnable(TIMER1_BASE, TIMER_A);
ROM_TimerEnable(TIMER2_BASE, TIMER_A);
ROM_TimerEnable(TIMER3_BASE, TIMER_A);
ROM_TimerEnable(TIMER0_BASE, TIMER_B);
ROM_TimerEnable(TIMER1_BASE, TIMER_B);
ROM_TimerEnable(TIMER2_BASE, TIMER_B);
ROM_TimerEnable(TIMER3_BASE, TIMER_B);
IntMasterEnable();
while(1)
{
// Loop forever while the timers run.
}
}
When I run this code the output of pins PC4 PC5 PC6 and PC7 are reduced in frequency (to 2000 KHz aprox ), and using the debuger I see that the interrupts of Timer0IntHandlerB, Timer1IntHandlerB, Timer2IntHandlerB, Timer3IntHandlerB never happen, I do not know why this is not working, my objetive is to generate 8 square signals at diferent frequencies... what migth be the problem??,
The start up file was updated to support the interruptions of the 8 timers.