This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Folks,
I develop a system, that consist of two embedded boards, connected together via SPI. The data transfer happens only master -> slave.
Master: EK-TM4C1294XL launchpad
Slave: TM4C123AH6P based custom board
I can only use the CCS' debugger to see what is going on, but I see, that data frames are received and read out by the slave from its buffer, but every time the data is ZERO.
Can anybody suggest me, what did I wrong, where should I found the solution, etc...
The related code of the Master
// Initialize the SPI1 related GPIOs MAP_GPIOPinConfigure(GPIO_PB4_SSI1FSS); MAP_GPIOPinConfigure(GPIO_PB5_SSI1CLK); MAP_GPIOPinTypeSSI(GPIO_PORTB_BASE, GPIO_PIN_4 | GPIO_PIN_5); MAP_GPIOPadConfigSet(GPIO_PORTB_BASE, GPIO_PIN_4 | GPIO_PIN_5, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD_WPU); MAP_GPIOPinConfigure(GPIO_PE4_SSI1XDAT0); MAP_GPIOPinConfigure(GPIO_PE5_SSI1XDAT1); MAP_GPIOPinTypeSSI(GPIO_PORTE_BASE, GPIO_PIN_4 | GPIO_PIN_5); MAP_GPIOPadConfigSet(GPIO_PORTE_BASE, GPIO_PIN_4 | GPIO_PIN_5, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD_WPU); // Initialize the SPI1 MAP_SSIConfigSetExpClk(SSI1_BASE, 120000000, SSI_FRF_MOTO_MODE_0, SSI_MODE_MASTER, 500000,16); MAP_SSIEnable(SSI1_BASE); // Sending data for (uint32_t index = 0; index < _dataOut.size(); ++index) { MAP_SSIDataPut(SSI1_BASE, _dataOut[index]); }
The related code of the Slave
// Initialize the SSI1 related GPIO ROM_GPIOPinConfigure(GPIO_PF0_SSI1RX); ROM_GPIOPinConfigure(GPIO_PF1_SSI1TX); ROM_GPIOPinConfigure(GPIO_PF2_SSI1CLK); ROM_GPIOPinConfigure(GPIO_PF3_SSI1FSS); ROM_GPIOPinTypeSSI(GPIO_PORTF_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3); ROM_GPIOPadConfigSet(GPIO_PORTF_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3, GPIO_STRENGTH_4MA, GPIO_PIN_TYPE_STD_WPU); // Initialize the SSI1 ROM_SSIConfigSetExpClk(SSI1_BASE, ROM_SysCtlClockGet(), SSI_FRF_MOTO_MODE_0, SSI_MODE_SLAVE, 500000, 16); ROM_SSIEnable(SSI1_BASE); // Reading from the buffer uint32_t data = 0; ROM_SSIDataGet(SSI1_BASE, &data); ROM_GPIOPinWrite(GPIO_PORTA_BASE, 0xFF, static_cast<uint8_t>(data)); ROM_GPIOPinWrite(GPIO_PORTB_BASE, 0xFF, static_cast<uint8_t>(data >> 8));
Can anybody help me?
Regards,
Norbert