Part Number: TMS570LS1227
There is a larger difference than expected in conversion result between the same input signal converted by ADC1 or ADC2. The followings relate the detailed configuration we have:
The ADC channel assignments:
ADC1 (Group2): ch5, ch6, ch7, ch13, ch22
ADC2 (Group2): ch5, ch6, ch7, ch8, ch9, ch12, ch14
As indicated in bold, the channels ADC1[22] and ADC2[6] are multiplexed on the same pin with an accurate 4.096 V shunt reference connected. The conversions are triggered simultaneously by a hardware trigger.
All ADC timing is identical with tACQ= 6 * tADCLK effectively resulting in simultaneous sampling of ADC1 and ADC2 each time according the sequence given above.
The following configuration settings are used:
VCLK1CLK=90MHz
ADCLK = 22.5MHz
12 bit conversion resolution
The theoretical conversion result of ADC1[22] and ADC2[6] would yield: ((4.0973 * 4096) / 5.0214)-0.5 = 3342
And the conversion results with the configuration described above are:
ADC1[22] = 3341 or 3342
ADC2[6] = 3334 or 3335 (too low value)
There is a larger difference than expected in conversion result between the same input signal converted by ADC1 or ADC2. In this case the difference is about 7 counts. However, when the timing is changed by changing the G2_ACQ value in the G2SAMP register (for ADC1 one clock period longer, for ADC2 one period shorter), the difference between the samples disappears (1 or 0 count) as expected, and given as followed:
ADC1[22] = 3341 or 3342
ADC2[6] = 3341 or 3342
On the other hand, without changing timing, we have tested one board at higher temperatures where the difference disappears at about 85 degrees Celsius.
A similar issue listed in the Silicon Errata (TMS570LS12x/11x Microcontroller Silicon Revision B) in page-9 with the name of ADC#1. There are two workarounds suggested in the errata. The first one is about the changing the timing similar to what we have tried.
Thus, we have the following questions:
1- Is the issue and the suggested work-around listed in the errata same as the issue we are having and described above?
2- Would you also suggest the workaround in the errata or another solution?
3- How can you explain not having the issue anymore when the temperature gets over 85 degrees Celcius?
Thanks in advance for your support!
Kind regards,
Ugur Keskin