Other Parts Discussed in Thread: UNIFLASH, HALCOGEN
hi,
i am using the TMS470MF06607 microcontroller.
i want to develop the SCI boot loader for this microcontroller. but in one of my previous mail, from the e2e forum i got the reply you have only CAN bootloader for this microcontroller.
in my previous mail i got some link for that CAN boot loader. from that link what ever the file i got it, i attached that file here also. can you please verify that one.
i have few doubt regarding that CAN & SCI boot loader.
1) i got that XDS100V2 emulator. through that ARM JTAG emulator i can flash my boot loader also into my microcontroller ??
2) from the CAN boot loader is it possible to convert it as a SCI boot loader.??? if its possible means how?
3) what i thought means in place of CAN TX & RX function, if i replace that SCI TX & RX function means the CAN boot loader will converted to SCI boot loader. is it correct or not ??
4)in that CAN boot loader zip file, i got one PDF also regarding that CAN boot loader. in that PDF they mentioned that b1_config.h file . from which folder i want to take that header file.
5) if i want to change that CAN boot loader to SCI boot loader means, in that CAN boot loader file from where i want to start . can you please suggest me little bit briefly.
regards
Arun Kumar.N4212.TMS470_BOOT.rar