Part Number: TM4C1290NCZAD
Other Parts Discussed in Thread: TIDA-00203, UNIFLASH
Tool/software: Code Composer Studio
Hello,
We are a systems integrator and had our Contact Manufacturer build TIDA-00203 CAN to Ethernet Boards. We have the can2enet demo programmed into each board and working. Each board does not have a MAC address. My question is:
1) Where do we get MAC addresses for these boards? Do we need need to go to http://standards.ieee.org/develop/regauth/oui36/index.html
MAP_EMACAddrSet(EMAC0_BASE, 0, (uint8_t *)pucMACAddr); from within Can2enet.c? Will that work?
b) Can we use UniFlash or LM Flash Programmer to program the MAC through the JTAG (right now USB is disabled since we flashed can2enet on each board and this demo does not enable USB). It looks like you can user "Other Utilities" under LM Flash Programmer to program a MAC. What "interface" do I choose for JTAG? Can we do it from UniFlash?
Please provide a couple of easy options for our end customer to program the MAC programatically from within can2enet.c and from LM Flash Programmer/Uniflash over JTAG? Or others?
Kind Regards,
Todd