Part Number: TM4C1230E6PM
Other Parts Discussed in Thread: ENERGIA, CC3100
Hi folks,
I am having difficulties in the following task: reading data from a light sensor.
I am working on a TM4C microcontroller and the light sensor is a Grove light sensor that came along with the Grove starter kit.
Problem 1 : workshop 14 of C-series covers light sensors but from the senshub booster pack
Problem 2: the manual that came along with the Grove pack covers reading from alight sensor but on energia and for TM1637 while I am using CCS and TM4C123. Here any insight on how to modify the code will be appreciated
Problem 3: I need to read data from a second light sensor, where to I connect (cables) the new light sensor, i.e. do I need a new Grove kit or any unused port will work?
PS:
1) I was using the workshops as a basis so I never used the grove kit before (for example, in TM4C I could use portD01 and portE45 for 2 light sensor but I do not know how the mapping works for the grove board)
2) I am new to TM4C but learning quickly
3) All available ressources: TM4c123G, LAUNCHXL-CC2620, Grove Starter kit, Educational BoosterPack MKII (this one has light sensors so it can be used as replacement for the grove), Touch LCD BoosterPack, CC3100 BoosterPack
Any help is welcome
Please feel free to notify me if any tag is missing or if it is the wrong forum section
Cheers