Part Number: RM48L952
Other Parts Discussed in Thread: HALCOGEN
Hello
One of my customers is asking about GIO Loopback testing :-
In the Safety Manual TI supplied for the RM48L952, there is a safety mechanism listed –
SW test of function using I/O checking
This is performed at power up and during normal operation. I can’t see a mechanism to perform a loopback internally.
Am I correct in thinking that this is a requirement shared with the circuitry around the microcontroller ? ie the external circuitry provides loopback of outputs to inputs and the inputs are stimulated by the external circuitry to make sure they are operable. ( This has been implemented)
Or is there a mechanism I haven’t been able to identify…
I notice there are loopback test features in some of the modules like N2HET and SPI but what is the recommended procedure for testing GIO.
Regards
Bob Bacon