Part Number: TM4C123GH6PM
I am trying to sample PE3 for a Sonar sensor, but my code never enters the ISR. I have updated my vector table with the "ADC_read_fxn" handler, but constantly just end up with "No source available for "0xfffffffe" errors. Any help would be greatly appreciated.
#include "sonar_init.h"
float distInch;
volatile unsigned int proflag=0;
void sonarInit(void)
{
//SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ);
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
SysCtlPeripheralReset(SYSCTL_PERIPH_ADC0);
ADCSequenceDisable(ADC0_BASE,3);
ADCSequenceConfigure(ADC0_BASE, 3, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceStepConfigure(ADC0_BASE, 3, 0, ADC_CTL_CH0 | ADC_CTL_IE | ADC_CTL_END);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_3);
ADCIntRegister(ADC0_BASE,3, &ADC_read_fxn);
ADCIntEnable(ADC0_BASE,3);\
ADCIntClear(ADC0_BASE, 3);
ADCSequenceEnable(ADC0_BASE,3);
IntMasterEnable();
}
void main(void)
{
sonarInit();
while(1){
if (proflag==0){
ADCProcessorTrigger(ADC0_BASE,3);
proflag=1;
}
}
}
void ADC_read_fxn(void)
{
ADCIntClear(ADC0_BASE,3);
while(!ADCIntStatus(ADC0_BASE, 3, false));
uint32_t rawADC;
ADCSequenceDataGet(ADC0_BASE, 3, &rawADC);
distInch=rawADC*102.4;
proflag=0;
}