Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: EK-TM4C123GXL
I want to use the USB VBUS for monitoring whether the device has connected and disconnected from the host. I'm a little confused after going through all the posts on the forum.
I am designing my own custom board and need a few clarifications. The silicon revision of the microcontroller is 7.
To connect the VBUS pin to PB1, I just need to add an RC filter to limit the rise time to below 2ns right? And for the times when the host is connected but the pin hasn't been configured in the USB mode, the voltage has to be limited to 3.3V, so I'm planning on using a simple voltage divider.
In summary, by using a voltage divider and RC filter I can connect the VBUS pin to PB1? Am I correct in inferring this?
Regards,
Shitij Avlani