Part Number: RM48L952
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
Hello,
In the HALCoGen 04.06.01, generate code from HALCoGen.
In SDRAM initialize function, the following statement is written in the function description. (emif_SDRAMInit() )
"As per the errata EMIF#5, EMIF SDRAM initialization must performed with EMIF clock below 40MHz."
But I can not find Errata EMIF # 5.
I am using the EMIF clock at 55 MHz, and I want to know whether it should be used below 40Mhz, or what conditions are there?